Part Number: TDA4AL-Q1
Hello, Expert.
I try to find parameter setting for CSI-RX DPHY in Linux device tree (DTS)
Do we support these parameret?
(1) phy-ths-settle-ns
I guess it should be time interval during which the HS receiver shall ignore any Data Lane HS transitions, starting from the beginning of tHS-SETTLE

(2) phy-ths-term-ns
I guess it should be time interval during which the HS-RX should ignore any transitions on the Data Lane, following a HS burst. The end point of the interval is defined as the beginning of the LP-11 state following the HS burst

(3) Could we configure "termination" enable/disable for CSI DPHY?
Thank You
Gibbs