Hi
I'd like to some clarification on the flags you can set in the AMMU on OMAP4430
for register SCACHE_MMU_LARGE_POLICY_i, there are several bits available to set, like
- L1_ALLOCATE and L2_POSTED
- L1_ALLOCATE and L2_POSTED
What does these mean?
also, for register SCACHE_OCP, there are three bits which I don't understand
WRALLOCATE, WRBUFFER and WRAP
What does these mean?
Furthermore, in chapter 5.4.2, the TRM says that that L1 consists of only 32kB, while in chapter 2.5 SL2->L1 is defined as a 128kB region. Why is this?
Chapter 5.4.2, it also says that L2 can be configured as both memory and cache. Can you explain how I do this?
BR
Niklas