Part Number: AM5749
We are developing a bare-metal application on the AM5749 processor. As we are using ECC memory, and ECC memory is only supported on the EMIF1 interface, the EMIF2 interface is unused. We wish to disable the EMIF2 module.
We have set CM_EMIF_EMIF2_CLKCTRL -> MODULEMODE to 0x0 (module disabled by software).
TRM "Table 3.241. CD_EMIF Modules Slave CLock-Management Modes and Control" states that disabling of the EMIF2 module via this register is supported, however following setting of MODULEMODE to 0x0 we see that CM_EMIF_EMIF2_CLKCTRL -> IDLEST remains at 0x1 (module performing transition) rather than moving to 0x3 (module disabled) as expected.
Please advise as to the correct procedure for disabling EMIF2.
Kind regards,
Stephen