Part Number: AM6442
Other Parts Discussed in Thread: ADC12DL040
Dear TI Support Team,
I am writing to inquire about the high-speed data acquisition capabilities of the AM64x Sitara processor, specifically using the PRU-ICSSG (Industrial Communication Subsystem) for a fast sampling application.
I am planning to interface an external ADC (specifically the ADC12DL040)or anyother to the AM64x Starter Kit. I have the following technical questions:
1. Sampling Rate: Can the PRU effectively handle a sampling rate of 40 MSPS for a 12-bit data stream?
2. Interface: Given the 40 MSPS requirement, which interface is recommended? I am currently looking at a Parallel CMOS interface using the PRU Expansion Header (J15). Is this the most efficient way to achieve single-cycle data capture?
3. Pin Mapping: Which specific pins on the header are optimized for this type of parallel data acquisition to ensure minimal latency and deterministic behavior?
4. Resource Recommendations: Are there any existing PRU firmware examples or application notes for high-speed parallel ADC interfacing on the AM64x?
I appreciate your guidance on the best practices for this implementation