I would like to run the C6747 at close to 375 MHz as possible. I am restricted to an already placed 24 MHz crystal for the clock input. I can do this by setting
pre-div to 2,
post-div to 1
Multiplier to 31, so core is 12*31=372 MHz
Div5 to 3 to give me 124 MHz (I am using 133 MHz SDRAM) on EMIF B
DIv2 defaults to 2 giving 186 MHz ti EDMA, McASP, SPI and UARTs
Div4 defaults to 4 giving 93 MHz on GPIO,, i2C
and I don't care about the other clocks.
Q1) However there is no pre-div setting in AISgen. So any way I can set pre-div?
Q2) Is 186 MHz a valid clock for the EDMA, McASP, SPI and UARTs.
Thanks,
Fawad