This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM620-Q1: AM620-Q1 TPM support

Part Number: AM620-Q1

Hi Team ,

 

Does AM620-Q1 support the TPM on chip? if not , suggest the discreat TPM  module.

 

Thank you.

  • Hello Shubham Vadnal,

    Thank you for the query.

    The AM62x processor family of device are HS-FS and the eFuse can be written to convert HS-FS to HS-SE.

    I suspect this is similar to the TPM but integrated into the processor.

    A LDO based VPP supply needs to be implemented On-Board or can be supplied from an external source controlled by SOC IO

    Regards,

    Sreenivasa