Part Number: AM2434
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
uart_uniflash.py allows to flash binaries to the flash on a EVM. UART is used as the transport or interface to send the file to flash to the EVM. When the uart_uniflash.py script is executed, a multi-stage process is initiated to program the external flash memory over UART. The below process occurs from the FLASH and OSPI perspective.