This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 NAND operation with CS2n



Asisting with a DM8168 board bring-up, and discoved that the NAND memory was inadvertently wired to use GPMC_CS2n chip select instead of GPMC_CS0n. Is it possible to use CS2n with NAND memory properly?

If so, what is the address modification needed in the GEL file to implement this?

Any information or advice appreciated! - Bruce

  • The TRM (SPRUGX8), sec 25.7.3 describes NAND boot requirements.  CS0 is the only chip select supported.  Boot code is in ROM, so can't be easily changed.  Requires new device spin, so not practical in this case.

    Regards.