Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH, TPS22965
Hello TI!
On the EVM Board for TDA4VH-Q1 the Power Switches for VDD_IO_3V3 and VDD_GPIORET_IO_3V3, respectively (U75 and U62, TPS22965NDSGR) are each rated for 6A max. But the sum of the onboard loads on these two supplies seems to require far less than 6A. In our case, we don´t even have USB, PCIe, eMMC or any external loads so the current demand on those two supplies are even lower in our design.
The Power Estimation Tool excel sheet does also not indicate any significant current demand by the TDA4VH itself on either of these two 3.3V supplies.
What is the reason for having such a high current rating on these two power switches on the EVM?
The answer would be input for us to see if we could step down in current rating on those two power switches in our design, or if there is something "hidden" that after all requires the switches to be able to handle as much as 6A, at least in peak situations?
Or is there perhaps some other switch property that is a consequence of an over-sized current rating, that is the actual property needed here?