Other Parts Discussed in Thread: TVP5158
Hi All,
Currently I have DVRRDK from udworks using McFW and we would like to implement below cases, please advice if it is feasible and guide on which portion has to be change:
1. Reduce 16 ch to 8 ch, thus reduce supported TVP5158 from 4 unit to 2 unit
2. Support IP camera stream in. (This is possible in old omx framework, but in McFW - 01.06.00.11, I do not see any similar example/code)
3. Support IP camera stream out. (This is available in old omx framework, but not in McFW 01.06.00.11)
4. Live view from 4 analog input, mosaic into one and streaming out
5. OSD overlay on video input (either from analog input or IP camera input)
6. Perform a snapshot of live view
Thank you very much.
Best regards,
Cheng