This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dvsdk 4.03 ,patch failed :Hunk #1 FAILED at 107.

Hi,

I upgrade dvsdk to dvsdk 4.3 ,and update the folder external/ti-dsp form https://gitorious.org/rowboat/external-ti-dsp/trees/rowboat-gingerbread-dsp . I compile the project ,when install the dvsdk ,it patch failed .It seems there is something wrong in the external/ti-dsp/patchs/..

My Dev-kit is GingerBread_2_3-DSP_DevKit_1_0 ,and the buid error is as follow:

========================= Press Space to Continue ==============================
Enter y if you accept ALL license agreements, else enter n. [y/n] y

GPLv3 Components Contained within SDK

This installation step is to inform you that there are software components within the SDK that are licensed as GPLv3. These software components are for development purposes only, and are intended to be removed before installing the application(s) code in your final product. For more information please refer to the Software Developer's Guide (SDG) at section GPLv3 Disclaimer.


========================= Press Space to Continue ==============================
Enter y if you accept above license agreements, else enter n. [y/n] y


Where do you want to install dvsdk? [/usr/local/dvsdk] /home/bakerhuang/MyWorkspace/myrowboat/external/ti-dsp/ti-dvsdk_dm3730-evm_04_03_00_06

Installing dvsdk...
Installing Files...                                                                
The following installation may take several minutes. A completed message will be shown
when done.
Installation complete.

The next steps guiding you how to start software development on the dm3730-evm is
available in the TMS320DM3730_Software_Developers_Guide.pdf available under
/home/bakerhuang/MyWorkspace/myrowboat/external/ti-dsp/ti-dvsdk_dm3730-evm_04_03_00_06/docs.
Patching DVSDK components for Android...
patching file Makefile
patching file Rules.make
patching file c6accel_1_01_00_07/config.bld
Hunk #1 succeeded at 76 with fuzz 2.
patching file c6accel_1_01_00_07/soc/Makefile
patching file c6accel_1_01_00_07/soc/app/Makefile
patching file c6accel_1_01_00_07/soc/app/timeObj.h
patching file c6accel_1_01_00_07/soc/c6accelw/Makefile
patching file codec-engine_2_26_02_11/config.bld
patching file codec-engine_2_26_02_11/packages/ti/sdo/ce/ipc/dsplink/package.bld
patching file codec-engine_2_26_02_11/packages/ti/sdo/ce/osal/linux/GT_config_posix.c
patching file codec-engine_2_26_02_11/packages/ti/sdo/ce/osal/linux/Thread_posix.c
patching file dsplink_1_65_01_05_eng/dsplink/gpp/src/api/Linux/_notify.c
patching file dmai_2_20_00_15/packages/config.bld
patching file dmai_2_20_00_15/packages/ti/sdo/dmai/Makefile
Hunk #1 FAILED at 107.
1 out of 1 hunk FAILED -- saving rejects to file dmai_2_20_00_15/packages/ti/sdo/dmai/Makefile.rej
patching file dmai_2_20_00_15/packages/ti/sdo/dmai/apps/Makefile.app
Failed get_tidsp.sh, aborting..
make: *** [dvsdk] Error 1

  • Baker Huang,

                I could understand your problem now. But porting DVSDK 4.03.00.06 to rowboat is in progress. So you must wait for few more days, or stick to DVSDK 4.02.00.06 itself.

                We will let you know on this post once this is done.

    Thanks & Regards,

    Velan

  • oh ,god .You shouldn't release this dvsdk until all is done or note us about this .It cost us lots time .But thank you all the same .

  • Baker Huang said:

    oh ,god .You shouldn't release this dvsdk until all is done or note us about this .It cost us lots time .But thank you all the same .

    Understood your frustration, but please note that the DVSDK is called Linux DVSDK, it has nothing to do with Android or Rowboat. Rowboat just uses it for H/W video decoding on DM37xx. So I don't see any issue of releasing 4.03 even if Rowboat does not support it yet.
    Also the Rowboat wiki page http://code.google.com/p/rowboat/wiki/DSP only says it supports 4.01 at the moment, so to get 4.03 working on Rowboat, you either have to wait until the Rowboat project completes the porting, or do the work by yourself.