This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X IBIS - DDRx section



Hi,

We want to use AM335X IBIS file for board analysis. AM355X IBIS file have much complexity its

DDR section. For data lines "Selector 2"  defines from Model_563 to Model 593 for slow and slowest

corners and from Model_627 to Model_658 for fast/fastest corners for 1.8V DDR2 buffers.

In addition to this every model has [number]* RExt.  This [number] have diffferent values : 1.00, 1.60, 1.14, 1.33,

0.88, 0.73, 0.67, 1.14, ......  What is the mean of [number] s and RExt ? I don't see these values are configurable

via register in TRM ? For input, there are many modes, FULL TERM [number]*Rext, Pull-up down, Pull -down,

Half thevenin.... How do data input buffers have different models on the processor? ODT is defined only RAMs

and not bidirectional signal. Or How can we set input termination schema for this device? 

Address and Clock lines have same complexity, too. 

RAM driver strengths  are defined in TRM for DDR2 as 0 and 1, DDR3 as RZQ/6 and RZQ7, LPDDR as 1/2, 1/4 or 1/8. But

how can we set relation to upper strength options to IBIS file?

Thanks, 

FERHAT

  • Hi!

    The meaning of the  [number]* RExt values can be found in the IBIS model.

    The driver strength can be set in I[2:0] section of the ddr_cmd0_ioctrl and ddr_cmd1_ioctrl and ddr_cmd2_ioctrl and ddr_data1_ioctrl and ddr_data0_ioctrl registers of the control module.

    driver strength I[2:0]
     1.60*RExt 5mA 000
     1.33*RExt 6mA 001
     1.14*RExt 7mA 010
     1.00*RExt 8mA 011
     0.88*RExt 9mA 100
     0.80*RExt 10mA 101
     0.73*RExt 11mA 110
     0.67*RExt 12mA 111

    The slew rate of the signals can be set in the same registers in the SR[1:0] section.

    slew rate SR[1:0]
    slowest 11
    slow 01
    fast 10
    fastest 00

    I have not found any information about the ODT settings (Half Thevenin, FULLTERM, Pull-down, Pull-up/down off). In the SDRAM_CONFIG register (EMIF4D register set) you can set the ODT remination values with reg_ddr_term[2:0].

    value reg_ddr_term[2:0]
    ODT off 000
    ODT with 75 Ohm 001
    ODT with 150 Ohm 010
    ODT with 50 Ohm 011

    But I don't know how to connect these with the IBIS model.
    Does anyone have more information?

    Best Regards,

    Balazs Ancsa 

  • Hi Balazs, 

    You are right to setting selection of drive strengths.But there is complexity input termination settings still. I have asked directly TI, but I

    did not received satisfiying answer. If any answers come back to me, I will share it on this page.

    Best Regards,

    FERHAT 

  • Hi!

    I could figure out the settings of the DDR controller (thanks for measurements)

    • The driver strength can be set in I[2:0] section of the ddr_cmd0_ioctrlddr_cmd1_ioctrlddr_cmd2_ioctrlddr_data0_ioctrl and ddr_data1_ioctrl registers of the control module.
    settingdriver strengthI[2:0]
    1.60*RExt 5mA 000
    1.33*RExt 6mA 001
    1.14*RExt 7mA 010
    1.00*RExt 8mA 011
    0.88*RExt 9mA 100
    0.80*RExt 10mA 101
    0.73*RExt 11mA 110
    0.67*RExt 12mA 111
    • The slew rate of the signals can be set in the same registers in the SR[1:0] section.
    slew rateSR[1:0]
    slowest 11
    slow 01
    fast 10
    fastest 00
    • The ODT settings can be set in the DDR_PHY_CTRL_1 and DDR_PHY_CTRL_1_SHADOW register in the reg_hpy_rd_local_odt[1:0] section.
    ODTreg_phy_rd_local_odt[1:0]
    Disabled 00
    Disabled 01
    Full 10
    Half 11
    • The memory settings can be set in the EMIF_SDRAM_CONFIG register (this will be transfered to the DDR memory during initialization)
      • ODT settings in reg_ddr_term[1:0] section
    ODTreg_ddr_term[1:0]
    Disabled 00
    75 Ohm 01
    150 Ohm 10
    50 Ohm 11
      • Drive settings in reg_sdram_drive[0] section.
    ODTreg_sdram_drive[0]
    Normal 0
    Reduced 1
  • If I am right, the reference manual has a mistake in the DDR_PHY_CTRL_1 register description.

    It says for the reg_hpy_rd_local_odt[1:0] bits that 0b01 is full thevenin ODT and 0b10 is disabled ODT.
    I have tried this settings it seems that 0b01 is the disabled ODT and 0b10 is full thevenin ODT.

    Could somebody verify this?

    Best Regards,
    Balázs 

  • Yes, Balazs, you are correct 0x01 is disabled, and 0x10 is full thevenin ODT.  Those will be fixed in the next TRM release. 

    Regard,s

    James

  • I'll add one additional piece of info to this already useful thread!  There are some models like this:

    [model]         Model_714

    |     Sub model VREF_NOTERM_PUPD_OFF_5PER_1P8

     

    [model]         Model_726

    |     Sub model LVCMOS_PUPD_OFF_5PER_1P8

     

    The "VREF" models refer to DDR2/DDR3 while the "LVCMOS" models refer to LPDDR.  This corresponds to the programming of ddr_io_ctrl.mddr_sel in the TRM (i.e. 0 for DDR2/DDR3 and 1 for LPDDR).

     

  • As we see it, in order to actually do a simulation we will have to:

                    1) read back the configuration registers over the JTAG interface.

                    2) parse the data comparing register addresses to data sheet to determine settings

                    3) coordinate our findings with our Hyperlynx guy to assist him in correctly configuring his simulation tools to our specific application.

    All this is labor intensive and prone to errors.

    Has anyone created a PC application that will read back the appropriate data, parse it, and generate an “application” specific IBIS model or creation a file that we can send to TI for “application” specific IBIS model creation.

  • Blake -- I would envision the process being the other way around, i.e. the hardware guy does the simulation and tells the software guy how he's supposed to configure the DDR.

    On a related note, I've created this wiki page to try and bring all this info together in one place:

    http://processors.wiki.ti.com/index.php/How_to_use_the_AM335x_IBIS_Models

    If nothing else, both the simulation/hardware engineer and the software engineer can both read the article to understand how they are expected to coordinate the activity.