Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829,
Hello TI,
is there any documentation that provides the information at which clock the M3 core in the WKUP domain (DMSC) is running? The data sheet only defines the maximum supported frequency, which is 333 MHz.
From measurements I know that the actual speed is actually 333 MHz, which is also conformed by this thread:
TDA4VM: EFUSE CLK and DMSC( M3 core) working clock - Processors forum - Processors - TI E2E support forums
However, for traceability I would need some official documentation that states how the clock is configured by the ROM code (which runs before the TIFS). Is this information anywhere available?
Regards
Thomas Dedler