Part Number: AM6442
Hi Champs,
My customer is working with TI U‑Boot on the AM64x platform and would like to clarify the flexibility around boot image naming.
From their current understanding and experimentation, the boot images appear to require the following fixed filenames:
- Tiboot3.bin
- Tispl.bin
- u-boot.img
Could you please confirm whether these image names are strictly required by the ROM boot flow / SPL handoff on AM64x, or if it is possible to customize or rename them through configuration (for example via U‑Boot build options, environment settings, or bootloader code changes)?
Additionally, if the naming is fixed:
- Which boot stages (ROM, SPL, etc.) explicitly depend on these filenames?
- Is this behavior consistent across all boot modes (OSPI, eMMC, SD)?
Any references to documentation or code locations that define this requirement would be greatly appreciated.
Regards,
Kien