Part Number: TDA4VM
Other Parts Discussed in Thread: AM2431
Hi,
I am using TI-ARAGO 2025.1 Yocto SDK on the TDA4VM EVM for qualification.
The TI FW images - tiboot3.bin, tispl.bin, sysfw.itb and u-boot.img are stored at specific offsets in the OSPI flash as per the reference design provided.
I am trying to setup the flash address map to be flexible and different the base reference design.
I have done this for the AM2431 via syscfg on TI CCS.
Since I am using Yocto SDK, I am trying to see how I can configure the syscfg for these individual binaries to provide the new flash offsets that I am planning to use.
Is there any mechanism built in the SDK to configure syscfg with recipes/append files/conf settings that I use to update these flash offsets ?
Thanks,
Prasanna