This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[HW] DM6467T V core down to 1.2V

Dear sirs:

The DM6467T power dissipation is much greater than DM6467. I am very interested in know how I can lower this power disipation.

Then, in the Excell spreadsheet for evaluate the power consumption for this chip, I find a note that implies that if I run the core at 900 MHz, I can lower the core voltage to 1.2V. I can't find documentation about that.

Anyone knows if it is true?. Anyone have some information about that?. I think that lowering VCC to 1.2V at 900 MHz core or below can be very interesting for power constrained applications.

 

If this is true, PCI can run at 66 MHz?

 

Thanks in advance