This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: SRAM ECC checking

Part Number: AM263P4-Q1
Other Parts Discussed in Thread: AM263P4

Hi.

I'm looking to implement ECC memory checks for RAM on the AM263P4 microcontroller to trigger an event on the ESM module. I've noted that there 6 ESM events for SRAM ECC (e.g. sram0_ecc_uncorr_pulse) but can't find any information on how these events are triggered. I've also noted that the soc_eccagg_uncorr_level ESM event looks to be used for RAM ECC monitoring, based on example code in the SDK files.

Could you clarify how ECC checking is set up for RAM, which ESM events are triggered for various fault conditions and any initialisation and fault injection methods used.

Thanks,

Carwyn

  • Hi ,

    Nilabh is currently OOO , please expect a delay in response of few days.

  • The AM263Px uses a hierarchical ECC aggregation architecture with two distinct error paths depending on the memory type. This is the key to understanding the events you're seeing.

    Two Error Paths to ESM

    1. R5F Core Memories (TCM, Icache, Dcache): These memories output ECC error signals on an internal EVNTBUS. The signals are aggregated in MSS_CTRL registers before being routed to the ESM [1]:

    Aggregated Signal
    ESM Event
    Type
    R5SS0_CORE0_CORR_ERRAGG
    ESM_LVL_EVENT_47
    Level
    R5SS0_CORE0_UNCORR_ERRAGG
    ESM_LVL_EVENT_48
    Level
    R5SS0_CORE1_CORR_ERRAGG
    ESM_LVL_EVENT_49
    Level
    R5SS0_CORE1_UNCORR_ERRAGG
    ESM_LVL_EVENT_50
    Level
    R5SS1_CORE0_CORR_ERRAGG
    ESM_LVL_EVENT_55
    Level
    R5SS1_CORE0_UNCORR_ERRAGG
    ESM_LVL_EVENT_56
    Level
    R5SS1_CORE1_CORR_ERRAGG
    ESM_LVL_EVENT_57
    Level
    R5SS1_CORE1_UNCORR_ERRAGG
    ESM_LVL_EVENT_58
    Level

    The correctable aggregator collects EVNTBUS signals [22, 23, 24, 25, 40, 41, 42] and the uncorrectable aggregator collects EVNTBUS signals [33, 34, 37, 38, 39] [2].

    2. System SRAM (L2OCRAM, MBOX, TPTC) — via ECC Aggregator 0: This is the path that maps to the soc_eccagg_uncorr_level event you observed. ECC Aggregator 0 protects these specific memories [3]:

    • L2OCRAM_BANK0 through L2OCRAM_BANK5 (6 banks)
    • MBOX_SRAM
    • TPTC_A0, TPTC_A1

    The aggregator outputs two Level-type signals to the ESM [4]:

    • SOC_ECCAGGR_UNCORR_LVL_0 — for double-bit (DED) uncorrectable errors
    • SOC_ECCAGGR_CORR_LVL_0 — for single-bit (SEC) correctable errors

    The six sram*_ecc_uncorr_pulse events you found likely correspond to the six L2OCRAM bank instances (BANK0–BANK5) before they are aggregated into the single SOC_ECCAGGR_UNCORR_LVL_0 signal. The SDK examples use the aggregated Level event because that's the final ESM interface.


    Initialization Sequence

    The SDK provides a clear initialization pattern. Here's the sequence for MSS L2 RAM as an example [5]:

    Step 1: Initialize the target memory

    /* Clear Done memory */
    SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_DONE_ADDR, 0xfu);
    /* Initialize MSS L2 memory (Bank 3 in this example) */
    SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_ADDR, SDL_ECC_MSS_L2_BANK_MEM_INIT);
    while(SDL_REG32_RD(SDL_MSS_L2_MEM_INIT_DONE_ADDR) != SDL_ECC_MSS_L2_BANK_MEM_INIT);
    /* Clear Done memory after init */
    SDL_REG32_WR(SDL_MSS_L2_MEM_INIT_DONE_ADDR, SDL_ECC_MSS_L2_BANK_MEM_INIT);

    Step 2: Clear any pre-existing error status

    c
    Collapse
    SaveCopy
    1
    SDL_REG32_WR(SDL_ECC_AGGR_ERROR_STATUS1_ADDR, 0xF0Fu);

    Step 3: Initialize ECC memory for the aggregator

    result = SDL_ECC_initMemory(SDL_SOC_ECC_AGGR, SDL_SOC_ECC_AGGR_MSS_L2_SLV2_ECC_RAM_ID);

    Step 4: Configure and initialize ESM with event bitmaps

    ⌄
    SDL_ESM_config ECC_Test_esmInitConfig_MAIN = {
    .esmErrorConfig = {1u, 8u},
    .enableBitmap = {0x00180000u, 0x00000000u, ...},
    .priorityBitmap = {0x00180000u, 0x00000000u, ...},
    .errorpinBitmap = {0x00180000u, 0x00000000u, ...},
    };
    result = SDL_ESM_init(SDL_ESM_INST_MAIN_ESM0,
    &ECC_Test_esmInitConfig_MAIN,
    SDL_ESM_applicationCallbackFunction, ptr);

    The bitmap values (0x00180000u = bits 19 and 20 in group 0) select which ESM events to enable, prioritize, and route to the error pin [5].

    Step 5: Initialize the ECC aggregator

    static SDL_ECC_MemSubType ECC_Test_MSS_L2_subMemTypeList[] = {
    SDL_SOC_ECC_AGGR_MSS_L2_SLV2_ECC_RAM_ID,
    };
    static SDL_ECC_InitConfig_t ECC_Test_MSS_L2_ECCInitConfig = {
    .numRams = 1,
    .pMemSubTypeList = &(ECC_Test_MSS_L2_subMemTypeList[0]),
    };
    result = SDL_ECC_init(SDL_SOC_ECC_AGGR, &ECC_Test_MSS_L2_ECCInitConfig);

    Important: ECC aggregators should be configured at startup, after running BIST [6].


    Fault Injection

    The SDK provides SDL_ECC_injectError() for testing. For wrapper-type RAM IDs (like SRAM), you must access the memory after injection to trigger the ESM event — the hardware detects the error during the read operation [7].

    Single-bit (SEC) error injection:

    SDL_ECC_InjectErrorConfig_t injectErrorConfig;
    injectErrorConfig.pErrMem = (uint32_t *)(0x70100008u); /* MSS_L2 address */
    injectErrorConfig.flipBitMask = 0x002; /* Flip 1 bit */
    result = SDL_ECC_injectError(SDL_SOC_ECC_AGGR,
    SDL_SOC_ECC_AGGR_MSS_L2_SLV2_ECC_RAM_ID,
    SDL_INJECT_ECC_ERROR_FORCING_1BIT_ONCE,
    &injectErrorConfig);
    /* Must access memory to trigger the error event */
    testLocationValue = injectErrorConfig.pErrMem[0];

    Double-bit (DED) error injection:

    injectErrorConfig.pErrMem = (uint32_t *)(0x70100008u);
    injectErrorConfig.flipBitMask = 0x03; /* Flip 2 bits */
    result = SDL_ECC_injectError(SDL_SOC_ECC_AGGR,
    SDL_SOC_ECC_AGGR_MSS_L2_SLV2_ECC_RAM_ID,
    SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE,
    &injectErrorConfig);
    testLocationValue = injectErrorConfig.pErrMem[0];

    ESM Callback handling:

    When the ESM fires, your callback receives the error details. Use SDL_ECC_getESMErrorInfo() and SDL_ECC_getErrorInfo() to identify the exact memory, RAM ID, and bit offset, then clear the pending interrupt [5]:

    SDL_ECC_getESMErrorInfo(esmInst, intSrc, &eccmemtype, &eccIntrSrc);
    SDL_ECC_getErrorInfo(eccmemtype, eccIntrSrc, &eccErrorInfo);
    SDL_ECC_clearNIntrPending(eccmemtype, eccErrorInfo.memSubType,
    eccIntrSrc, SDL_ECC_AGGR_ERROR_SUBTYPE_INJECT,
    eccErrorInfo.injectBitErrCnt);
    SDL_ECC_ackIntr(eccmemtype, eccIntrSrc);

    For R5F ATCM/BTCM specifically, you also need to enable ECC and the event bus before initialization [5]:

    SDL_ECC_UTILS_enableECCATCM();
    SDL_UTILS_enable_event_bus();

    The MSS_CTRL registers (R5SS*_CPU*_ECC_CORR_ERRAGG_MASK, _STATUS, _STATUS_RAW) control masking and status for the R5F memory error aggregation [2].


    To help refine this further, it would be helpful to know:

    • Whether you need to monitor specific SRAM banks (e.g., only certain L2OCRAM banks) or all RAM types
    • Whether you need both correctable (SEC) and uncorrectable (DED) error handling, or only uncorrectable
    • The exact ESM event numbers and bitmap positions for the individual sram*_ecc_uncorr_pulse events — these aren't fully mapped in the available SDK documentation and may require consulting the device-specific ESM event table in the TRM
    • Whether the six individual SRAM pulse events can be monitored directly at the ESM or only through the aggregated SOC_ECCAGGR Level signals

    1. AM263Px TRM - MSS_CTRL Hardware Requests (Table 6-10)
    2. AM263Px TRM - R5 Memory ECC Error Event Interrupt Aggregator
    3. AM263Px TRM - Device modules with ECC Aggregator (Table 13-256)
    4. AM263Px TRM - ECC Aggregator Event Requests (Table 13-255)
    5. MCU+ SDK AM263Px - SDL ECC Page
    6. MCU+ SDK AM263Px - SDL ECC API
    7. MCU+ SDK AM263Px - ECC MSS L2 Example
  • Hi Nilabh,

    Thanks for providing the above information and clarifying the purpose of those six SRAM ECC events for the ESM.

    Could you clarify, for the initialization sequence above, do steps 1-3 need to be performed in the bootloader before the application is transferred from flash memory to RAM?

    Thanks,

    Carwyn

  • Yes doing it in SBL insures that the check is done before application starts to boot.