This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Input Output access in Microcontroller M4F in AM6252

Part Number: AM625

Dear TI Team,

I am currently working on a project that involves accessing GPIOs using the M4F core on the AM6252 platform. I would like to understand how many GPIOs are available for access and control from the M4F core.

It would be helpful if you could also provide any relevant details regarding GPIO mapping, limitations, or configuration considerations specific to the M4F core.

Looking forward to your guidance.

Regards,
N. Eswara Rao

  • Hi,

    I am currently working on a project that involves accessing GPIOs using the M4F core on the AM6252 platform. I would like to understand how many GPIOs are available for access and control from the M4F core.

    The M4F core can access all the available GPIO in MAIN and MCU domain. Not all the pins are available in MCU/MAIN domain.

    Please refer to section 4.9.1.1 GPIO Unsupported Features of device TRM to see what all pins are available and not available.

    It would be helpful if you could also provide any relevant details regarding GPIO mapping, limitations, or configuration considerations specific to the M4F core.

    Please refer device TRM for all details. Also refer https://www.ti.com/lit/ab/spradk0/spradk0.pdf. 

    Also refer section 10.1.5 GPIO Interrupt Handling of TRM for GPIO interrupt routing.

    Regards,

    Tushar