Part Number: OMAP-L138
Hello,
Currently I am using an OMAPL138EZWT3, and there are some new requirements that may require the use of Secure Boot and JTAG disable. Looking at the documentation for the OMAP-L138 specficially SPRUGQ9, Processor Data sheet, and Technical Reference Manual. I see that the processor does indeed support these features, but further research is showing that its only supported on specific SKUs of the OMAP. I am not seeing any concrete specific information that confirms this SKU supports the potentially required features.
Can I get a confirmation that my processor supports these features? If it does not support them is their a secure enabled processor SKU directly equivalant to the one I am using?