Hi
I have TI814X based own board with 1GB of RAM. The details of main processor chip are as follows-:
TI8148-GP rev 2.1;;;;; part no is:: X8148X3874BCYE 1CZDCL9
I am trying to evaluate Android 2.3 devkit 2.0 on this board.
I have successfully build all the components and prepared the SD card.
The kernel booted successfully. but while loading hdvpss firmware the board just hanged up. Please find the serial port booting logs in attached file.
So I tried to load the frmware by command line by interrupting normal android booting sequence. The board still hanged up.
Following are the serial port debug messages of the command I have executed.
/system/bin/syslink/procmgrapp_release 2 /system/bin/syslink/c6a814x_hdvpss.xem3 0
ProcMgrApp sample application
Entered SysLinkSamples_startup
SysLinkSamples_osStartup
Entered ProcMgrApp_startup
ProcMgr_attach status: [0x0]
After attach: ProcMgr_getState
state [0x1]
ProcMgr_load status: [0x3046000]
After load: ProcMgr_getState
state [0x3]
ProcMgr_start passed [0x6a85000]
(board hanged after this)
Please note that I have successfully run ezsdk_dm814x-evm_5_03_01_15 on this board and seen matrix GUI on HDMI display.
Can somebody suggest me what is going wrong.
Regards,
Prashant.