Other Parts Discussed in Thread: AM3517
Hi,
Our customer are using AM3517 and planning to use newest SDK(v5.03.02)
and Arago Root File System.
I have question about Arago Root File System for AM3517.
How do you build Arago Root File System which are appropriate to SDKv5.03.02 ?
Is it right with the following repositories to clone?
git clone git://arago-project.org/git/projects/arago-amsdk.git
git clone git://arago-project.org/git/projects/arago-oe-amsdk.git
git clone git://arago-project.org/git/arago-bitbake.git
Or just build the arago environment according to the procedure of the URL as follows?
And able to get Arago RootFile System which are appropriate to newest SDK ?
http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment
best regards,
Challenger