Other Parts Discussed in Thread: AM3715
Hi,
Has anyone tried to measure a power on omap3_evm mistral board and linux images from:
http://processors.wiki.ti.com/index.php?title=AM/DM37x_Low_Power_Standby_Support.
There is written that VDDS_IO + VDDS_MEM + Memory Supply (J28) during standby mode is 0.09 mV so power is 1.6 mW on this line.
I measured this voltage using the images given from TI (http://processors.wiki.ti.com/images/a/a5/AMDM37x_standby_image.zip, http://processors.wiki.ti.com/images/8/88/Ramdisk.gz) and I can't achieve such value. I observed 1 mV, so it is much higher than value from the site.
Of course measuring manner is not perfect - but it is hard to believe that the multimeter can mix up so much. There is 0 or 0.1 mV on VDD2 and VCORE.
I try to estimate minimal power consumption of AM3715 Processor Module (AM3715 Processor with PoP memory Hynix (H8KDS0UN0MER-4EM) and the question is:
what is the lowest voltage level on VDDS_IO + VDDS_MEM +... which can be achieved.
I also tried with kernel from git://gitorious.org/rowboat/kernel branch: rowboat-kernel-2.6.37 SHA1ID: 1236e9fe8d7ce11ad71bfee391759528c0601fbf. The J28 (IO + mem) is 1.3 mV. (but not all power domains have to be put to low state etc. )
My soc rev. is ES1.2
Regards,
Karol