Hello,
I am having a problem that I cannot figure out
I am on DVSDK 4.02 using the built in Gstreamer.
can you look at my log please? http://pastebin.com/J9zQczDe
Every time I try to play video from rtspsrc I get "fatal bit error"
This is from 2 different cameras AND it was working in DVSDK 2.1
any help would be greatly appreciated
when I run that pipe I can view the "top" command and see that memory is reporting 200%+ for gst-launch
Also, for videotestsrc I see 39% memory and 99% CPU
this is on a DM368
Its almost like Gstreamer just wants to use memory from kernel and not CMEM. I have kernel memory at 60M from boot args.
Any help in the right direction would be greatly appreciated!!!
I have also posted at the Gstreamer TI forum
https://gstreamer.ti.com/gf/project/gstreamer_ti/forum/?_forum_action=ForumMessageBrowse&thread_id=4649&action=ForumBrowse&forum_id=187