This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Ref: [FAQ] AM2434: Custom Flash Attach Database

Part Number: AM2434

Ref: [FAQ] AM2434: Custom Flash Attach Database

Would it be correct to say that these devices are all supported by the TI SBL in the latest SDK ? 

Or are you providing this information so that the TI SBL can be user modified?

  • Hi Andrew,

    The devices mentioned in the FAQ are all the devices that have been used by previous customers and validated. These can be used with the TI SBL, however its always recommended to run the basic OSPI Flash IO example in the latest SDK to test whether Flash operations- erase,write, read are working correctly with the custom Flash device.

    Regards,

    Aryamaan Chaurasia

  • That's not what I asked, 

    Does the SDK support all of these devices without requiring modification, or is this information provided so that end users can modify the SDK ? 

    I am more interested in the SBL than the runtime. 

  • By default, the MCU+ SDK only supports Serial NOR OSPI Flash - S28HS512T and Serial NOR QSPI Flash  - S25HL512T from Infineon and NAND OSPI Flash - W35N01JWTBAG.

    The Flash parts mentioned in the FAQ are not supported by the MCU+ SDK by default, hence, the FAQ contains the values for Flash.

    The information is provided so that the users can modify the MCU+ SDK.

    Regards,

    Aryamaan Chaurasia