Part Number: AM6422
Dear TI Support,
I want to start with XDP_ZEROCOPY with our Board with AM6422 on a Port connected via ICSSG.
I found out that there is support for it in the mainline Kernel from November 20, 2025. History for drivers/net/ethernet/ti/icssg/icssg_prueth.c - torvalds/linux · GitHub 
I see that these commits are also in the TI Trees, e.g. in 11.02.13-rt: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/?h=11.02.13-rt&id=2aecd04861c5d6b9c6f9ed592e6c6bbf59b85140
In our current TI-Kernel 09.01.00.001-rt these commits are not inlcuded, as these commits are never, so I need to switch the kernel anyway.
I would prefer using the SLTS kernel 6.12 from the CIP: kernel/git/cip/linux-cip.git - Civil Infrastructure Platform stable kernel branches
The icssg_prueth.c driver there sees commits older and never than the required patch series adressing XDP_ZEROCOPY: kernel/git/cip/linux-cip.git - Civil Infrastructure Platform stable kernel branches
Is TI going to push the Commits for XDP_ZEROCOPY for pru_icssg to the CIP Kernel? If yes, is there a schedule for this?
Thanks for your reply!
BR
Daniel