Hi
I am trying to connect DM6437 EVM On board Emulator (SD DSK USB Emulator) with PC through mini USB cable.
While i am trying to connect the EVM board with CCS v3.3 through the option DEBUG -> Connect, it shows the following error
Error Connecting the target
Error : 0x80002240/- 1041
Fatal error during: initialization, OCS, Control
Device Driver: Problem with emulation controller
Kindly tell me whether it is possible to communicate CCS with EVM board through ON Board Emulator or not.
If yes for ON board emulator, what are the settings i have to do in CCS setup while connecting the board
If not, Please tell me is there any other way to communicate with the board?
Help me to sort out this problem.