Other Parts Discussed in Thread: MSP430F5438
Hallo Everyone,
i want to develop an application on the MSP430f5438 with Code Composer, and i want to use the RTOS " SYS/BIOS".
i have some question about SYS/BIOS, i hope some one can answer it:
1- can SYS/BIOS be compiled with the Eclipse?
2- does SYS/BIOS support reading and writing on a SD-Memory card with file system, that is compatible to windows?
3- is there a bluetuth-stack in SYS/BIOS, with wich is it possible to make a serial connection " for example via RS232" ?
4- is there a grafical windows-system in SYS/BIOS?
5- is there a debugger in SYS/BIOS to monitor the rtos and the tasks.?
6- can the division of the memory in stack and heap be known at anytime? is there is a way to monitor the division into stack and heap at anytime?
Best Regards,
Mohammad