Other Parts Discussed in Thread: OMAP3530
Hi,
I am using the u-boot version 2011 patch level 09 . When i booting the u-boot through JTAG i am getting following :
u-boot 2011.09-dirty (Feb 13 2012 - 11:17:42)
OMAP3530-GP ES3.1, CPU-OPP2, L3-165MHz, Max CPU Clock 720 mHz
OMAP3 Beagle board + LPDDR/NAND
I2C: ready
DRAM: 64 MiB
NAND: 512 MiB
MMC: OMAP SD/MMC: 0
NAND read from offset 260000 failed -74
*** Warning - readenv() failed, using default environment
In: serial
Out: serial
Err: serial
Beagle Rev C4
timed out in wait_for_pin: I2C_STAT=0
I2C read: I/O error
Unrecognized expansion board: 0
Die ID #6f54000400000000040398d316019007
Net: Net Initialization Skipped
No ethernet found.
Hit any key to stop autoboot: 0
OMAP3 OBBC #
In the beagle board u-boot in the NAND flash is erased. I just loaded the u-boot elf into beagle board through JTAG (CCS) and run it .What is the above marked error .How resolve it.
Thanks
bhimesh