Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hi,
GPIO0_60

GPIO1_60




The GPIO1_60 do not correspond
Regards,
Cesar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hi,
GPIO0_60

GPIO1_60




The GPIO1_60 do not correspond
Regards,
Cesar
Hi cesar.xu,
I am able to see the issue as well. It looks like all of the GPIO pins that are shared with OLDI0 are broken. I have let our development team know.
In the meantime, the offset/macro for the device tree should be:
J722S_IOPAD(0x027c, PIN_INPUT, 7)
You will also need to set the pinmux for GPIO1_61, because it is the pair for OLDI0_A4P/N
J722S_IOPAD(0x0280, PIN_INPUT, 7)
Datasheet excerpt:
"The GPIO functionality of these pins is configured by setting MUXMODE = 7 for both PADCONFIG registers of each OLDI pair. The positive pin's PADCONFIG register controls the ST_EN and PULLUDEN for the positive and negative pin. Only a pulldown is available on these pins and the PULLUDEN is active high."
Best,
Jared
Hi Cesar,
Please refer to the latest datasheet.
To configure these within the SysConfig PinMux Tool, please add a OLDI_GPIO instance on the lefthand side in the latest version of the tool and consider Jared's comment. Example: 
Regards,
Mark