Part Number: AM62L
I am working on BeagleBadge, based on TI AM62L, using the K3 vendor kernel 6.12.57-vendor-edge-k3. I am extending drivers/i2c/busses/i2c-omap.c so an AM62L I2C adapter can register a Linux I2C slave backend and still temporarily act as an I2C master/initiator.
The immediate test setup uses two AM62L OMAP I2C instances on the same board:
- J6 is
/dev/i2c-1, controller instance20010000.i2c - J7 is
/dev/i2c-3, controller instance20020000.i2c - J6 and J7 are physically shorted together
- Linux
i2c-slave-testunitis used as the target/slave backend - No external I2C devices are connected for this test
Validated working cases:
- J6 target at
0x30, J7 initiator: true SMBus block-proc-call works - J7 target at
0x30, J6 initiator: true SMBus block-proc-call works - repeated-start version reads work in the single-target reverse-topology case
The remaining failing case is when both adapters are target-capable at the same time:
- J6 target at
0x30 - J7 target at
0x31
After both targets are registered and bound, either initiation direction times out:
i2ctransfer -f -y 3 w1@0x30 0x00 i2ctransfer -f -y 3 r1@0x30 i2ctransfer -f -y 1 w1@0x31 0x00 i2ctransfer -f -y 1 r1@0x31
All four commands time out, even though each single-target topology works.
Driver changes already tested:
- added OMAP
reg_slave/unreg_slaveplumbing - clear stale master state before returning to slave listen mode
- switch from the slave IRQ mask to the normal master IRQ mask when an adapter with a registered slave backend initiates a master transfer
- on AM62L/IP-v2, clear
I2C_IRQENABLE_CLRbefore writing the next role's desired interrupt mask, becauseI2C_IRQENABLE_SETonly sets bits
The last change did remove the previous stale IRQ mask problem:
- before: failing dual-listener logs showed accumulated
ie=0x661f - now: logs show cleaned masks such as
ie=0x61fandie=0x601f Transmit underflowis no longer observed
But the dual-listener case still times out in both directions.
The relevant current kernel state is:
components/ti-linux-kernel:eb09330dc065Clear OMAP IRQ enables before role mask writescomponents/armbian-build:b17e72e32Add OMAP IRQENABLE clear patch- tested artifact:
6.12.57-S22fb-D0000-Pb163-C2876Hb496-HK01ba-Vc222-Be8e3-R448a - booted kernel:
Linux beaglebadge 6.12.57-vendor-edge-k3 #27 SMP PREEMPT Tue May 5 16:45:44 UTC 2026 aarch64 GNU/Linux
Question:
For AM62L OMAP I2C IP-v2, is there an additional required sequence when two controllers on the same physical I2C bus are both left in target/slave listen mode, but either one may temporarily become master?
Specifically:
- When switching a target-capable adapter from slave-listen mode into master mode, besides clearing
I2C_IRQENABLE_CLR, clearing status, settingMST, and restoring slave-listen mode afterward, is there another register or FIFO state that must be reset? - Is it expected that an OMAP I2C controller with own address enabled can interfere with another controller's transaction to a different target address on the same bus?
- Should
OA/ target addressing be disabled while an adapter is initiating a master transfer, then restored afterward? - Are there AM62L-specific constraints for using two OMAP I2C instances as multi-controller participants on the same physical bus?
The attached/pasted reproduction log includes:
- exact commands
uname -a- target backend status
- exit status for each
i2ctransfer dmesglines containingomap_i2c,Transmit underflow,Arbitration lost, timeout,slave irq,isr-master, andmaster-enter
The goal is not to debug the Linux slave-testunit backend itself. The single target cases prove that target mode and true SMBus block-proc-call work in both directions. The problem only appears when both OMAP adapters are simultaneously registered as target-capable listeners on the shorted J6/J7 bus.
Kernel patches are at https://github.com/just-kitting/ti-linux-kernel/tree/badge-snake