This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux serial console of AM335x-PSP-04.06.00.03 + Sitara Linux SDK version 5.03.01.00 on Beaglebone Rev. A3



Hi,

I installed AM335x-PSP-04.06.00.03 kernel + Sitara Linux SDK version 5.03.01.00 file system on my Beaglebone Rev. A3 board. But linux login prompt never appear from the serial console(I used ttyO1 instead of default ttyO0). I need to enter linux console to change DHCP setting of ethernet port to static IP.

Here is log and anyone help? Thanks

-----------------------logs-------------------------------------------------------------------------------------------------------------------------------------

U-Boot SPL 2011.09 (Feb 13 2012 - 17:28:14)
Texas Instruments Revision detection unimplemented
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2011.09 (Feb 11 2012 - 18:23:02)

I2C:   ready
DRAM:  256 MiB
WARNING: Caches not enabled
No daughter card present
NAND:  HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0
*** Warning - readenv() failed, using default environment

Net:   cpsw
Hit any key to stop autoboot:  0
SD/MMC found on device 0
reading uEnv.txt

152 bytes read
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage

2877216 bytes read
## Booting kernel from Legacy Image at 82000000 ...
   Image Name:   Linux-3.1.0-00117-gc9c405d
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2877152 Bytes = 2.7 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

[    0.000000] Linux version 3.1.0-00117-gc9c405d (x0029463@psplinux060) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Wed Dec 14 15:39:28 IST 2011
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 32512
[    0.000000] Kernel command line: console=ttyO1,115200n8 root=/dev/mmcblk0p2 mem=128M rootwait
[    0.000000] PID hash table entries: 512 (order: -1, 2048 bytes)
[    0.000000] Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
[    0.000000] Memory: 128MB = 128MB total
[    0.000000] Memory: 123864k/123864k available, 7208k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     DMA     : 0xffa00000 - 0xffe00000   (   4 MB)
[    0.000000]     vmalloc : 0xc8800000 - 0xf8000000   ( 760 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc051f000   (5212 kB)
[    0.000000]       .init : 0xc051f000 - 0xc0558000   ( 228 kB)
[    0.000000]       .data : 0xc0558000 - 0xc05ad080   ( 341 kB)
[    0.000000]        .bss : 0xc05ad0a4 - 0xc05e7620   ( 234 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz
[    0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[    0.000000] Console: colour dummy device 80x30
[    0.000190] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.059027] pid_max: default: 32768 minimum: 301
[    0.059151] Security Framework initialized
[    0.059251] Mount-cache hash table entries: 512
[    0.059618] CPU: Testing write buffer coherency: ok
[    0.064146] print_constraints: dummy:
[    0.064515] NET: Registered protocol family 16
[    0.064854] GPMC revision 6.0
[    0.066855] OMAP GPIO hardware version 0.1
[    0.068994] omap_l3_smx omap_l3_smx.0: couldn't find resource
[    0.069734] omap_mux_init: Add partition: #1: core, flags: 0
[    0.072647]  omap_i2c.1: alias fck already exists
[    0.074081]  omap2_mcspi.1: alias fck already exists
[    0.074291]  omap2_mcspi.2: alias fck already exists
[    0.096644] bio: create slab <bio-0> at 0
[    0.098368] SCSI subsystem initialized
[    0.100747] usbcore: registered new interface driver usbfs
[    0.101083] usbcore: registered new interface driver hub
[    0.101289] usbcore: registered new device driver usb
[    0.101642] registerd cppi-dma Intr @ IRQ 17
[    0.101657] Cppi41 Init Done Qmgr-base(c883a000) dma-base(c8838000)
[    0.101668] Cppi41 Init Done
[    0.119133] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[    0.121092] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.122133] Switching to clocksource gp timer
[    0.129110] Switched to NOHz mode on CPU #0
[    0.137522] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.137721] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[    0.138854] musb-hdrc musb-hdrc.0: USB OTG mode controller at c880a000 using DMA, IRQ 18
[    0.139026] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[    0.140023] musb-hdrc musb-hdrc.1: USB OTG mode controller at c880c800 using DMA, IRQ 19
[    0.140424] NET: Registered protocol family 2
[    0.140619] IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.140900] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[    0.140987] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.141043] TCP: Hash tables configured (established 4096 bind 4096)
[    0.141056] TCP reno registered
[    0.141068] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.141094] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.141273] NET: Registered protocol family 1
[    0.141563] RPC: Registered named UNIX socket transport module.
[    0.141576] RPC: Registered udp transport module.
[    0.141585] RPC: Registered tcp transport module.
[    0.141595] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.141815] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.149873] VFS: Disk quotas dquot_6.5.2
[    0.149938] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.150492] msgmni has been set to 241
[    0.151245] io scheduler noop registered
[    0.151258] io scheduler deadline registered
[    0.151328] io scheduler cfq registered (default)
[    0.152491] Could not set LED4 to fully on
[    0.193218] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.194851] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.195204] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.685440] console [ttyO1] enabled
[    0.689542] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.697269] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.704964] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.712645] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.728727] brd: module loaded
[    0.736763] loop: module loaded
[    0.740212] i2c-core: driver [tsl2550] using legacy suspend method
[    0.746710] i2c-core: driver [tsl2550] using legacy resume method
[    0.753133] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.812174] No daughter card found
[    0.815766] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.830966] Board name: A335BONE
[    0.834340] Board version: 00A3
[    0.837609] The board is a AM335x Beaglebone.
[    0.842491]  omap_hsmmc.0: alias fck already exists
[    0.850011] mtdoops: mtd device (mtddev=name/number) must be supplied
[    0.857049] omap2-nand driver initializing
[    0.861548] OneNAND driver initializing
[    0.912186] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    0.918637] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    0.925804] davinci_mdio.0: probed
[    0.929351] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[    0.938046] CAN device driver interface
[    0.942041] CAN bus driver for Bosch D_CAN controller 1.0
[    0.948376] usbcore: registered new interface driver cdc_ether
[    0.954656] usbcore: registered new interface driver cdc_subset
[    0.960871] Initializing USB Mass Storage driver...
[    0.966161] usbcore: registered new interface driver usb-storage
[    0.972439] USB Mass Storage support registered.
[    0.977303] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.982952] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.990774] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.997873] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.005417] usb usb1: Product: MUSB HDRC host driver
[    1.010589] usb usb1: Manufacturer: Linux 3.1.0-00117-gc9c405d musb-hcd
[    1.017490] usb usb1: SerialNumber: musb-hdrc.1
[    1.022991] hub 1-0:1.0: USB hub found
[    1.026926] hub 1-0:1.0: 1 port detected
[    1.032004] mousedev: PS/2 mouse device common for all mice
[    1.038984] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[    1.045685] omap_rtc: already running
[    1.049829] i2c /dev entries driver
[    1.093404] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.100091] cpuidle: using governor ladder
[    1.104880] cpuidle: using governor menu
[    1.112641] usbcore: registered new interface driver usbhid
[    1.118454] usbhid: USB HID core driver
[    1.123467] usbcore: registered new interface driver snd-usb-audio
[    1.131468] ALSA device list:
[    1.134614]   No soundcards found.
[    1.138155] oprofile: hardware counters not available
[    1.143429] oprofile: using timer interrupt.
[    1.147901] nf_conntrack version 0.5.0 (1935 buckets, 7740 max)
[    1.154533] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.160180] TCP cubic registered
[    1.163577] NET: Registered protocol family 17
[    1.168215] can: controller area network core (rev 20090105 abi 8)
[    1.174750] NET: Registered protocol family 29
[    1.179380] can: raw protocol (rev 20090105)
[    1.183843] can: broadcast manager protocol (rev 20090105 t)
[    1.189785] Registering the dns_resolver key type
[    1.194774] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.202783] ThumbEE CPU extension supported.
[    1.207987] _regulator_get: mpu.0 supply mpu not found, using dummy regulator
[    1.215547] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=720000000 v=1260000)on vddmpu
[    1.224721] omap2_set_init_voltage: unable to set vdd_mpu
[    1.232320] Detected MACID=40:5f:c2:76:89:d4
[    1.241371] omap_rtc omap_rtc: setting system clock to 2011-12-16 08:45:41 UTC (1324025141)
[    1.250710] Waiting for root device /dev/mmcblk0p2...
[    1.282858] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.293207] mmc0: new high speed SDHC card at address b368
[    1.299569] mmcblk0: mmc0:b368 USD   3.75 GiB
[    1.306034]  mmcblk0: p1 p2
[    7.168632] kjournald starting.  Commit interval 5 seconds
[    7.529463] EXT3-fs (mmcblk0p2): using internal journal
[    7.534934] EXT3-fs (mmcblk0p2): recovery complete
[    7.904904] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[    7.912132] VFS: Mounted root (ext3 filesystem) on device 179:2.
[    7.918763] Freeing init memory: 228K
INIT: version 2.86 booting
Please wait: booting...
Error opening /dev/fb0: No such device
Starting udev
[    8.437386] udevd (574): /proc/574/oom_adj is deprecated, please use /proc/574/oom_score_adj instead.
[   12.003618] alignment: ignoring faults is unsafe on this CPU.  Defaulting to fixup mode.
Remounting root file system...
Caching udev devnodes
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1625: No soundcards found...
Configuring network interfaces... [   18.129879]
[   18.129889] CPSW phy found : id is : 0x7c0f1
[   18.136705] PHY 0:01 not found
eth0      no wireless extensions.

udhcpc (v1.13.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Hardware abstraction layer hald
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: lighttpd.
2011-12-16 08:46:08: (log.c.166) server started
/
/
Starting Matrix GUI application.
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
        binutils-dev
        binutils-symlinks
        binutils
        gdbserver

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************


  • What happens if you press ENTER on the console?

    also, I'm not sure why you changed the console to ttyO1but you might want to check you /etc/inittab file to make sure you spawn a console to ttyO1 since by default you probably only have one being spawned on ttyO0.  Look for a line like:

    S:2345:respawn:/sbin/getty 115200 ttyO0

    Chase

  • Beaglebone uses ttyO0. Also since it uses USB as the console, you need to switch the console,

    assuming you are using Teraterm on Host, use New connection and select com port related to Beagle bone (This new com port will be created when UAR Tcable is connected to HOST)

    Regards

    Gururaja

  • when I press ENTER on the console, the teminal response me with a new line. I do not have a usb link to beaglebone usb port and this is the reason why I want to switch to UART1. I connect my host WINDOWS 7 serial port through beaglebone UART1.

    And here is uEnv.txt file that I used for linux kernel:

    bootargs=console=ttyO1,115200n8 root=/dev/mmcblk0p2 mem=128M rootwait
    bootcmd=mmc rescan; fatload mmc 0 0x82000000 uImage; bootm 0x82000000
    uenvcmd=boot

    Since this serial link UART1 is the only one path that I can talk to beaglebone board(we do not have a DHCP server so beaglebone ethernet wont work by default), there is no way for me to access linux console and make any changes there.

  • What serial port are you trying to use on the beaglebone?  There is no serial port on the board aside from the USB serial port.

    What happens when you use console=ttyO0,115200n8 as the console?

    Lastly, if you want to change the inittab you can do that by mounting the rootfs partition on a Linux host and modifying the file there.

    Chase

  • Hi, Chase

    Finally I mounted rootfs on tf card to my linux host and change inittab file as you suggested. Now I can enter linux console on ttyO1 now.

    Thanks

    Weidong