This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: ICSSG switch mode initialization issues

Part Number: TMDS64EVM
Other Parts Discussed in Thread: AM6442

Hello,

I have a problem with proper initialization of ICSSG two port ethernet switch mode. I'm using commands from documentation for latest SDK. One thing I cannot overcome is dropping multicast packets, SMV traffic to be specific (ether type 0x88BA). My setup is as below:

PC <-> EVM (switch mode) <-> AM6442 custom board

Custom board is sending PTP packets, SMV packets and as an additional test ICMP ping. If I strictly follow switch mode configuration order on EVM described in documentation (with physical interfaces already up):

ip link add name br0 type bridge
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
bridge vlan add dev br0 vid 1 pvid untagged self

and watch traffic on Wireshark on PC, I can see different behavior in differenct scenarios:

  • enable switch mode with PC on EVM eth1, custom board on EVM eth2 (already connected on boot) - in this case I can see SMV, PTP ICMP traffic is forwarded both ways, also after switching cables on eth1 and eth2 ports
  • enable switch mode with custom board on EVM eth1, PC on EVM eth2 - first ~20 SMV packets forwarded, then all SMV dropped, PTP and ICMP forwarded properly
  • configure switch mode and connect eth afterwards - all SMV dropped, PTP and ICMP forwarded properly

I tried playing with VLAN configuration, FDBs, MDBs, multicast flooding and cut through forwarding, but these setting didn't seem to have any influence on filtering once SMV dropping is noticed.

Another thing is if after configuring switch mode and noticing SMV being dropped I first disable both physical interfaces and then bring them back up (which causes ICSSG firmware to reload), I can see that whole traffic including SMV is being forwarded but only from port that was brought up later to the one that was brought up first, to be specific.:

ifconfig eth1 down
ifconfig eth2 down
ifconfig eth1 up
ifconfig eth2 up

will cause only forwarding traffic from eth2 to eth1. EVM itself still responds to ping on both ports, but both devices connected to EVM can't reach each other.

I see this behavior of switch mode on both EVM board running image from 12.0 SDK and custom AM6442 board with Yocto build using kernel 6.18.13 and icssg0 instead of icssg1 used by EVM.

The main question is do I miss something in the configuration of switch mode? Is it ICSSG binary or driver bug? Also which behavior is expected, dropping multicast traffic or forwarding it? Any other think I could test or check to find a root cause of these differences?

Best regards,
Mateusz

  • Hi Mateusz,

    I tested the scenario below and was unable to reproduce it with Generic Ethernet:

    configure switch mode and connect eth afterwards - all SMV dropped, PTP and ICMP forwarded properly

    Host PC: 

    $ ./pack_gen 01:80:8b:77:ce:bf 128 1000 0

    1000 packets were sent at 128 bytes each. Are you seeing the following message in the logs once the link is up?

    root@am64xx-evm:~# [ 102.823723] icssg-prueth icssg1-eth eth1: Link is Up - 1Gbps/Full - flow control off
    [ 102.831985] br0: port 1(eth1) entered blocking state
    [ 102.837063] br0: port 1(eth1) entered forwarding state
    [ 102.887913] icssg-prueth icssg1-eth eth2: Link is Up - 1Gbps/Full - flow control off
    [ 102.895838] br0: port 2(eth2) entered blocking state
    [ 102.900904] br0: port 2(eth2) entered forwarding state

    BR
    JC

  • Hi JC,

    Yes, I can confirm I can see these logs. Attached a few more of dmesg logs in case something interesting is there:

    [  151.637636] audit: type=1006 audit(1748545982.709:2): pid=853 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
    [  151.637669] audit: type=1300 audit(1748545982.709:2): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe80560d8 a2=1 a3=1 items=0 ppid=1 pid=853 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" key=(null)
    [  151.637684] audit: type=1327 audit(1748545982.709:2): proctitle="(systemd)"
    [  158.231415] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [  158.261946] br0: port 1(eth1) entered blocking state
    [  158.262034] br0: port 1(eth1) entered disabled state
    [  158.262101] icssg-prueth icssg1-eth eth1: entered allmulticast mode
    [  158.264858] icssg-prueth icssg1-eth eth1: entered promiscuous mode
    [  158.265846] audit: type=1700 audit(1748545989.334:3): dev=eth1 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
    [  158.270596] audit: type=1300 audit(1748545989.334:3): arch=c00000b7 syscall=211 success=yes exit=40 a0=3 a1=ffffc90627c8 a2=0 a3=1 items=0 ppid=860 pid=871 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=ttyS2 ses=4294967295 comm="ip" exe="/usr/sbin/ip.iproute2" key=(null)
    [  158.270637] audit: type=1327 audit(1748545989.334:3): proctitle=6970006C696E6B00736574006465760065746831006D617374657200627230
    [  158.362098] br0: port 2(eth2) entered blocking state
    [  158.362198] br0: port 2(eth2) entered disabled state
    [  158.362256] icssg-prueth icssg1-eth eth2: entered allmulticast mode
    [  158.364795] remoteproc remoteproc7: stopped remote processor 3008a000.txpru
    [  158.364823] remoteproc remoteproc16: stopped remote processor 30084000.rtu
    [  158.364832] remoteproc remoteproc13: stopped remote processor 300b4000.pru
    [  158.364842] remoteproc remoteproc8: stopped remote processor 3008c000.txpru
    [  158.364851] remoteproc remoteproc15: stopped remote processor 30086000.rtu
    [  158.364860] remoteproc remoteproc14: stopped remote processor 300b8000.pru
    [  158.368691] remoteproc remoteproc13: powering up 300b4000.pru
    [  158.374260] remoteproc remoteproc13: Booting fw image ti-pruss/am64x-sr2-pru0-prusw-fw.elf, size 45708
    [  158.374308] remoteproc remoteproc13: unsupported resource 5
    [  158.374341] remoteproc remoteproc13: remote processor 300b4000.pru is now up
    [  158.374389] remoteproc remoteproc16: powering up 30084000.rtu
    [  158.378718] remoteproc remoteproc16: Booting fw image ti-pruss/am64x-sr2-rtu0-prusw-fw.elf, size 34188
    [  158.378780] remoteproc remoteproc16: remote processor 30084000.rtu is now up
    [  158.378827] remoteproc remoteproc7: powering up 3008a000.txpru
    [  158.381384] remoteproc remoteproc7: Booting fw image ti-pruss/am64x-sr2-txpru0-prusw-fw.elf, size 39340
    [  158.381451] remoteproc remoteproc7: remote processor 3008a000.txpru is now up
    [  158.381496] remoteproc remoteproc14: powering up 300b8000.pru
    [  158.384651] remoteproc remoteproc14: Booting fw image ti-pruss/am64x-sr2-pru1-prusw-fw.elf, size 45868
    [  158.384694] remoteproc remoteproc14: unsupported resource 5
    [  158.384727] remoteproc remoteproc14: remote processor 300b8000.pru is now up
    [  158.384773] remoteproc remoteproc15: powering up 30086000.rtu
    [  158.387637] remoteproc remoteproc15: Booting fw image ti-pruss/am64x-sr2-rtu1-prusw-fw.elf, size 33424
    [  158.387693] remoteproc remoteproc15: remote processor 30086000.rtu is now up
    [  158.387740] remoteproc remoteproc8: powering up 3008c000.txpru
    [  158.390687] remoteproc remoteproc8: Booting fw image ti-pruss/am64x-sr2-txpru1-prusw-fw.elf, size 37828
    [  158.390749] remoteproc remoteproc8: remote processor 3008c000.txpru is now up
    [  158.394064] icssg-prueth icssg1-eth eth2: entered promiscuous mode
    [  158.394660] audit: type=1700 audit(1748545989.434:4): dev=eth2 prom=256 old_prom=0 auid=4294967295 uid=0 gid=0 ses=4294967295
    [  158.397225] audit: type=1300 audit(1748545989.434:4): arch=c00000b7 syscall=211 success=yes exit=40 a0=3 a1=ffffe2dda038 a2=0 a3=1 items=0 ppid=860 pid=877 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=ttyS2 ses=4294967295 comm="ip" exe="/usr/sbin/ip.iproute2" key=(null)
    [  158.397347] audit: type=1327 audit(1748545989.434:4): proctitle=6970006C696E6B00736574006465760065746832006D617374657200627230
    [  165.028985] icssg-prueth icssg1-eth eth1: Link is Up - 100Mbps/Full - flow control off
    [  165.029212] br0: port 1(eth1) entered blocking state
    [  165.029239] br0: port 1(eth1) entered forwarding state
    [  169.188912] icssg-prueth icssg1-eth eth2: Link is Up - 100Mbps/Full - flow control off
    [  169.189144] br0: port 2(eth2) entered blocking state
    [  169.189197] br0: port 2(eth2) entered forwarding state


    I now checked with image from SDK 11.02.08.02, the behavior is the same as on SDK 12.0 for me.

    Could you please verify if in your case it's any different with SMV multicast MAC? One between 01:0C:CD:04:00:00 and 01:0C:CD:04:01:FF. Our size of frame is 136 bytes, 4800 frames per second.

    Also worth noticing, I now see that in switch mode PRP supervision packets with MAC 01:15:4E:00:01:00 are forwarded from one port to another while these with SMV multicast MAC (e.g. 01:0C:CD:04:00:03) are not.

    Best regards,
    Mateusz

  • Hi Mateusz,

    Can you confirm if this packet structure is fine?

    • configure switch mode and connect eth afterwards - all SMV dropped, PTP and ICMP forwarded properly

    I tried this with above scenario, still the packets are forwarded for me.

    BR
    JC

  • Hi JC,

    Can you confirm if this packet structure is fine?

    At least destination MAC and packet type look ok.

    One thing I now see compared to traffic that I have is VLAN tagging that is present in our testing SMV packages. Could it be that the issue is not multicast type, but actually VLAN tagging? Example:


    Also, could you please confirm if this scenario is reproducible, with switch mode enabled and cables connected:

    first disable both physical interfaces and then bring them back up (which causes ICSSG firmware to reload), I can see that whole traffic including SMV is being forwarded but only from port that was brought up later to the one that was brought up first


    Best regards,
    Mateusz

  • Hi Mateusz, 

    Also worth noticing, I now see that in switch mode PRP supervision packets with MAC 01:15:4E:00:01:00 are forwarded from one port to another while these with SMV multicast MAC (e.g. 01:0C:CD:04:00:03) are not.

    Thanks for the details I will try today.

    BR
    JC

  • Hi JC,

    Waiting for the update.

    In the meantime I have one more question, how is it with forwarding PTP packets? I would like to configure the device to work as a switch with PTP Boundary Clock functionality - one port acting as PTP master, another one as PTP slave, not forwarding PTP packets between ports so so quite different compared to the example in switch mode documentation. I'm going through settings in the documentation but can't figure out how to prevent forwarding PTP packets.

    Best regards,
    Mateusz

  • Hi Mateusz, 

    I was able to reproduce the issue on my Linux setup. This appears to be a configuration/command-related issue, which I investigated internally. The same firmware works correctly with RTOS, confirming that this is unrelated to the PRU firmware.

    Regarding the command used to setup bridge mode: I suspect this

    bridge vlan add dev br0 vid 1 pvid untagged self

    Regarding the additional findings - if you wish to continue testing, VLAN ID 1 does work. To understand why, VLAN ID 1 functions because the bridge is registered for VLAN ID 1, and the untagged flag instructs it to strip the VLAN tag. This behavior is consistent when I run above command - meaning VLAN ID 1 is received and forwarded to other ports as untagged traffic, as defined by the above command.

    I also attempted to configure VLAN ID 0 using the same command, however, it still does not work. I am currently looking into this internally and the investigation is still ongoing.

    BR
    JC

  • I also attempted to configure VLAN ID 0 using the same command, however, it still does not work. I am currently looking into this internally and the investigation is still ongoing.

    Just a note that on CPSW hardware VLAN ID 0 is always reserved and used for priority tagging purposes. I'm unsure if it is the same for ICSSG so worth JC to look into

    -Daolin

  • Hello,

    This behavior is consistent when I run above command - meaning VLAN ID 1 is received and forwarded to other ports as untagged traffic, as defined by the above command.

    That's quite a clarification, thanks. Indeed I managed to control forwarding once the traffic used other VLAN ID. So from my understanding every VLAN ID that could be used for SMV traffic from other devices (excluding VLAN ID 0 at this moment) in the network has to be set explicitly configured for on the device in order to forward it without stripping the VLAN tag, is that correct?

    Also could you clarify my doubts regarding PTP traffic?

    I would like to configure the device to work as a switch with PTP Boundary Clock functionality - one port acting as PTP master, another one as PTP slave, not forwarding PTP packets between ports so so quite different compared to the example in switch mode documentation. I'm going through settings in the documentation but can't figure out how to prevent forwarding PTP packets.


    Best regards,
    Mateusz

  • Hi Mateusz,

    I would like to configure the device to work as a switch with PTP Boundary Clock functionality - one port acting as PTP master, another one as PTP slave, not forwarding PTP packets between ports so so quite different compared to the example in switch mode documentation. I'm going through settings in the documentation but can't figure out how to prevent forwarding PTP packets.

    Have you tried skipping the configuration steps to enable switch mode? My understanding and from past tests I've ran is that if you run ptp4l on each of the three devices connected in a line, the middle device doesn't necessarily have be enabled in switch mode for PTP boundary clock to work, assuming you have configured the ptp4l config file correctly.

    So from my understanding every VLAN ID that could be used for SMV traffic from other devices (excluding VLAN ID 0 at this moment) in the network has to be set explicitly configured for on the device in order to forward it without stripping the VLAN tag, is that correct?

    If CPSW ethernet is used, yes I believe your understanding is correct. If ICSSG ethernet, JC can most likely validate it performs the same.

    -Daolin

  • So from my understanding every VLAN ID that could be used for SMV traffic from other devices (excluding VLAN ID 0 at this moment) in the network has to be set explicitly configured for on the device in order to forward it without stripping the VLAN tag, is that correct?

    True.

    BR
    JC

  • Hello,

    Have you tried skipping the configuration steps to enable switch mode? My understanding and from past tests I've ran is that if you run ptp4l on each of the three devices connected in a line, the middle device doesn't necessarily have be enabled in switch mode for PTP boundary clock to work, assuming you have configured the ptp4l config file correctly.

    Unfortunately, enabling switch mode is the main functionality that the device would need and ptp4l boundary clock mode is a result of that requirement.

    Best regards,
    Mateusz

  • Hi Mateusz,

    Run this command in the bridge/BC, then things should work. I verified at my end.

    bridge mdb add dev br0 port br0 grp 01:80:c2:00:00:0e  permanent vid 1

    BR
    JC

  • > > 01:80:c2:00:00:0e 

    Above LLDP multicast MAC address is P2P reserved MAC - this be causing a rogue delay response, Which packets are getting forwarded in your case?

    You can also run the same command for the SYNC message MAC address from the Grandmaster (GM).

    If you have any further questions, please raise a separate E2E query and attach the relevant BC.cfg and OC.cfg configuration files.

    BR
    JC

  • Hello JC,

    Which packets are getting forwarded in your case?

    In my case it's Pdelay_Req, Pdelay_Resp and Pdelay_Resp follow up messages (ptp4l running in P2P mode). I now tried both:

    bridge mdb add dev br0 port br0 grp 01:80:c2:00:00:0e permanent vid 1
    bridge mdb add dev br0 port br0 grp 01:1b:19:00:00:00 permanent vid 1

    and I see these MACs have been added when checking with
    bridge mdb list

    but still on other port of the bridge I can see forwarded request/response/follow up messages and synchronization is breaking.

    Should further discussion now be moved to a new thread?

    Best regards,
    Mateusz

  • Hi Mateusz, 

    Should further discussion now be moved to a new thread?

    Yes, please

    Probably you can verify and close this one Slight smile

    BR
    JC

  • Also please attach the PTP OC and BC config files you are using.

    BR
    JC

  • Maybe one more question before closing:

    I also attempted to configure VLAN ID 0 using the same command, however, it still does not work. I am currently looking into this internally and the investigation is still ongoing.

    Could I somehow track or be notified with progress of the investigation?

    Best regards,
    Mateusz

  • I also attempted to configure VLAN ID 0 using the same command, however, it still does not work. I am currently looking into this internally and the investigation is still ongoing.

    Okay, you can then leave this thread open until this is addressed


    BR
    JC