This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB wifi 3070

Hello,

I have a usb wireless (3070 Ralink) and using montavista kernel 2.6.18 for dmva1. The error below appears like 2 out of 10 reboot of my system and most of the time it works OK. The driver was loaded first (as a module) during the system boot up and I have no idea where to start digging the problem.

Any idea?.

Regards,

john

insmod: page allocation failure. order:3, mode:0x0
Mem-info:
DMA per-cpu:
cpu 0 hot: high 6, batch 1 used:5
cpu 0 cold: high 2, batch 1 used:0
DMA32 per-cpu: empty
Normal per-cpu: empty
HighMem per-cpu: empty
Free pages:         848kB (0kB HighMem)
Active:3095 inactive:4095 dirty:35 writeback:0 unstable:0 free:212 slab:601 mapped:368 pagetables:29
DMA free:972kB min:848kB low:1060kB high:1272kB active:12252kB inactive:16380kB present:45056kB pages_scanned:0 all_unreclaimable? no
lowmem_reserve[]: 0 0 0 0
DMA32 free:0kB min:0kB low:0kB high:0kB active:0kB inactive:0kB present:0kB pages_scanned:0 all_unreclaimable? no
lowmem_reserve[]: 0 0 0 0
Normal free:0kB min:0kB low:0kB high:0kB active:0kB inactive:0kB present:0kB pages_scanned:0 all_unreclaimable? no
lowmem_reserve[]: 0 0 0 0
HighMem free:0kB min:128kB low:128kB high:128kB active:0kB inactive:0kB present:0kB pages_scanned:0 all_unreclaimable? no
lowmem_reserve[]: 0 0 0 0
DMA: 19*4kB 23*8kB 50*16kB 1*32kB 1*64kB 0*128kB 0*256kB 0*512kB 0*1024kB 0*2048kB 0*4096kB 0*8192kB 0*16384kB = 1156kB
DMA32: empty
Normal: empty
HighMem: empty
Swap cache: add 0, delete 0, find 0/0, race 0+0
Free swap  = 0kB
Total swap = 0kB
Free swap:            0kB
11264 pages of RAM
353 free pages
2601 reserved pages
601 slab pages
5861 pages shared
0 pages swap cached
 ERROR in Alloc Bulk buffer for RxContext!
---> RTMPFreeTxRxRingMemory
- RTMPFreeTxRxRingMemory
ERROR!!! Failed to allocate memory - TxRxRing
 RTMPAllocAdapterBlock, Status=3
rt2870: probe of 1-1:1.0 failed with error -1