This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fetch packet exception thrown from trampolined functions



Hi,

I'm having a problem with "Fetch packet exception" errors as below.

  |  A0=0x1 A1=0x0
| A2=0x8000b251 A3=0x3
| A4=0xe A5=0x8cd487d0
| A6=0x8cc56f4c A7=0x3f9921fb
| A8=0x0 A9=0x4356a1b1
| A10=0x0 A11=0x4000
| A12=0x8cd437e0 A13=0x8cc8dc20
| A14=0xf8 A15=0x8cd483e8
| A16=0x8cd437e0 A17=0x0
| A18=0x8cc81354 A19=0x20
| A20=0x8cd432a0 A21=0x0
| A22=0x8cd437e0 A23=0x800138ac
| A24=0x0 A25=0x0
| A26=0x8cd498b0 A27=0x0
| A28=0x8cc68c4c A29=0x1
| A30=0x4 A31=0x8cd4a2e0
| B0=0x1 B1=0x0
| B2=0x1 B3=0x8c82c9f0
| B4=0x0 B5=0x3ff00000
| B6=0x54442d18 B7=0x3f1921fb
| B8=0x0 B9=0x3fe00000
| B10=0x0 B11=0xbff00000
| B12=0x0 B13=0x3ff00000
| B14=0x8cd4f048 B15=0x80009e78
| B16=0x0 B17=0x40000000
| B18=0xe42bde38 B19=0x3fefe24f
| B20=0x28 B21=0x1083a06c
| B22=0xf B23=0x0
| B24=0xffffffff B25=0x40a99747
| B26=0x2434802d B27=0x0
| B28=0x0 B29=0x1
| B30=0x0 B31=0x2
| NTSR=0x1000f
| ITSR=0x0
| IRP=0x0
| SSR=0x0
| AMR=0x0
| RILC=0x0
| ILC=0x0
| Exception at 0x8cc03dc0
| EFR=0x2 NRP=0x8cc03dc0
| Internal exception: IERR=0x12
| Fetch packet exception
| Resource conflict exception
| ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x00000000, sp = 0x80009e78.
| xdc.runtime.Error.raise: terminating execution
| Done

The debug build runs fine, this happens only in release build. When I traced into the place where the exception was thrown, it was always a trampolined function as below. When I looked at the address of both $TRAM$S$$_Somefunction and Somefunction, the contents hadn't changed since the program load time. I checked/unchecked "L1P Cache" and "L2 Cache" check box in the memory browser, still I didn't see any difference.

          $Tramp$S$$_SomeFunction:
8cc03dc0: 01174410 B.S1 SomeFunction (PC+571936 = 0x8cc8f7e0)

Is there any guidance to debug this kind of issue? Sorry about a very vague description, but this was a part of a large program and was difficult to single out this issue. 
BTW, there are a lot of functions that were trampolined, but most of them didn't have any issue. Only a few function suffered from this exception.

The versions of the tools were as follows.

CCStudio 5.1
CGTools 7.3.1
MCSDK 02_00_05_17.
EVM: evm6678le_xds560v2

Thanks,
  • NRP could be pointing after the exception occurred. What are the instructions in a couple of fetch packets above this instruction and the rest of the fetch packet after this instruction? In other words, please show the disassembler window for 0x8cc03d80-0x8cc03ddf.

    The address in B3 is usually the return address of a function call, so you can look back to that address to see where this came from. That could help with tracking down the actual cause.

    An exception like this should never occur in compiler-generated code. Causes can be stack overflow, memory corruption from invalid/incorrect pointers, and such.

    Regards,
    RandyP

  • Thank you very much for your comment Randy.

    Below is the disassebler window for 0x8cc03d80-0x8cc03ddf that you requested.I've replaced some irrelevant symbol names with *****.

    The area 0x8cc03ddc-0x8cc03d7 might not be a valid code, but it had not changed since the application was loaded to the memory.


    $Tramp$S$$__cxa_guard_release:
    8cc03d70: 01231810 B.S1 __cxa_guard_release (PC+596160 = 0x8cc95620)
    8cc03d74: 00008000 NOP 5
    8cc03d78: 00000000 NOP
    8cc03d7c: 00000000 NOP
    $Tramp$S$$_ZN10*******_:
    8cc03d80: 01221810 B.S1 ***** (PC+594112 = 0x8cc94e40)
    8cc03d84: 00008000 NOP 5
    8cc03d88: 00000000 NOP
    8cc03d8c: 00000000 NOP
    $Tramp$S$$_Znwj:
    8cc03d90: 010C5C10 B.S1 operator new (PC+549600 = 0x8cc8a060)
    8cc03d94: 00008000 NOP 5
    8cc03d98: 00000000 NOP
    8cc03d9c: 00000000 NOP
    ~__class_type_info:
    8cc03da0: 00100FD8 MV.L1 A4,A0
    8cc03da4: D0000290 [!A0] B.S1 $C$L13 (PC+20 = 0x8cc03db4)
    8cc03da8: C122DC10 [ A0] B.S1 operator delete (PC+595680 = 0x8cc95480)
    8cc03dac: D08C6362 [!A0] BNOP.S2 B3,3
    8cc03db0: 00000000 NOP
    $C$L13:
    8cc03db4: 00002000 NOP 2
    8cc03db8: 00000000 NOP
    8cc03dbc: 00000000 NOP
    $Tramp$S$$_****************_:
    8cc03dc0: 01174410 B.S1 ********** (PC+571936 = 0x8cc8f7e0)
    8cc03dc4: 00008000 NOP 5
    8cc03dc8: 00000000 NOP
    8cc03dcc: 00000000 NOP
    $P$T0$2:
    8cc03dd0: 00000001 NOP
    8cc03dd4: 00000001 || NOP
    8cc03dd8: 00000000 || NOP
    8cc03ddc: FFFFFFFF .word 0xffffffff
    8cc03de0: FFFFFFFF || .word 0xffffffff
    8cc03de4: FFFFFFFF || .word 0xffffffff
    8cc03de8: 00000000 || NOP
    8cc03dec: 00000001 NOP
    $Tramp$S$$_****************_:
    8cc03df0: 01227010 || B.S1 ***** (PC+594816 = 0x8cc95160)
    8cc03df4: 00008000 NOP 5
    
    

    I also realized that the code that throws the internal exception was a part of a constructor, which was called from a C++ code like below. The code has been running fine on C64x+ compiled with CGTool v6.0.

    const classA& classA::only ()

    {

    static classA instanceA(paramters);

    return instanceA;

    }

    I really appreciate your help.

    Thanks,



  • Hi Randy,

    FYI, below is an excerpt from the map file. As you see below, the data between 8cc03dd0 and  8cc03dec was not corrupted, but actually coming from a .const.1 data section.

    80000000    80000000    0c800000   00000000    rw-
    80000000 80000000 0c800000 00000000 rw- .sysmem
    8c800000 8c800000 00403de0 00403de0 r-x
    8c800000 8c800000 00403de0 00403de0 r-x .text.1
    8cc03dd0 8cc03dd0 00000070 00000070 r-x
    8cc03dd0 8cc03dd0 00000020 00000020 r-- .const.1
    8cc03df0 8cc03df0 00000010 00000010 r-x .text.2
    8cc03e00 8cc03e00 00000010 00000010 r-- .const.2
    
    
    Thanks,
  • Since the yellow highlighting seems to have changed the indentation, it is not quite as easy to figure out what the relationships are with the lines. But I think I understand.

    However, it looks like the .text.1 section should use the range from 8c800000-8cc03ddf while the .const.1 section overlaps with it by using 8cc03dd0-8cc03def. They overlap by 16 bytes, or am I misreading something here?

    If that overlap is my mistake or does not really matter for some reason, and the area from the previous post that looked like corrupt code is really just constant data, then are we any closer to solving your problems?

    Regards,
    RandyP

  • I was also wondering why there was the 16 byte overlap of .text.1 and .const.1. An excerpt from the map file was copy-pasted and is not a mistake.

    I understand that the exception was thrown because was a data from .const section got into fetch packet. The strange 16 byte overlap might be indicating that the linker is doing something wrong with laying out .code and .text sections. As a work around for now, we are trying to put .text and .const into one contiguous sections respectively and reduce the chance of const data getting into .text segment. But if this is an issue in the linker, can we expect a fix in the near future release?

    Best regards,