Other Parts Discussed in Thread: AM3715, TPS65950
Hi,
We are using TI_Android_GingerBread_2_3_4_Sources. And the Platform is based on AM3715 and TPS65950.
We need the USB to work in HOST mode and it should supply 5V in VBUS line. From the TPS65950 TRM it is clear that writing a 1 to the DRVVBUS bit of OTG_CTRL register will drive 5V on VBUS.
I would like to know how this is done from the code?
Which is the corresponding .c file in kernel?
Iam a newbie to Android. Thanks for any input you may have.
Thanks & Regards in Adv.
Vivek