This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Boot Configuration pull up/down resistors

Hi,


What are recommended pull up/down resistor values for "SYS_BOOT" pins of AM3359.
We will be using LCD pins which are multiplexed with the boot pins.

In the schematics of the ICE BOARD and BeagleBone the SYS_BOOT pins are
pulled up up/down through 100K,±1% resistors.
Are resistors(100K) with tolerance of ±1% necessary?


Regards.