Other Parts Discussed in Thread: AM3359
Hi,
I am making a PRU application that does data collection a number of reasonbly high speed (50 kHz kind of range) external A/D converters. The PRU is going to basically collect the data, and do minimal processing on it, but the real idea is to get it pushed into circular buffers so that the main processor can use them, with most of the data analysis taking place from higher level software running on linux.
My question is about DMA and the PRU.
The AM3359 PRU has
- Data Mem0 (8KB)
- Data mem1 (8KB)
- Shared RAM (12KB)
As I said in a previous post, I don't really understand why make the distinction, when either PRU can use either DMEM as well as shared memory (they all seem to talk through the 32-bit interconnect bus).
What I'm wondering is: if 12KB is enough, why would I bother with DMA at all, and just have the main CPU access shared RAM through the L3 or L4 (not sure which) interconnects? All the above memories are mapped into the same global address space, aren't they?
The DMA modes I have read about in the PRU examples all have DMA basically being memory-to-memory copy anyhow. If I could get the DMA to work differently, where the PRU could efficiently send a single byte at a time over DMA, I'd do that. I'm just not quite sre how.
--Chris