This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Guidance Required for Custom PCB Development Using TDA4VM (Linux + RTOS Heterogeneous Architecture)

Part Number: TDA4VM

Hello Team,

I am planning to develop a custom board based on the TDA4VM platform and would like guidance/recommendations from experts who have experience with hardware design, Linux/RTOS integration, and bring-up of custom boards using this SoC.

Project Overview

The system architecture is planned as follows:

  • Linux (A72 cores) will primarily handle:
    • Data logging
    • High-level application management
    • Storage handling
    • Communication interfaces
    • Diagnostics and monitoring
  • RTOS (R5F/C7x cores) will handle:
    • Real-time sensor acquisition
    • IMU + compass + altimeter fusion
    • Upstream system data processing
    • Motor control and deterministic tasks
    • Real-time communication/control loops

The system is intended for a robotics/autonomous embedded application where deterministic real-time behavior is critical while Linux handles non-real-time workloads.

Areas Where Guidance Is Required

1. Custom Hardware Design Recommendations

I would like to understand best practices for designing a custom PCB around TDA4VM:

Power Architecture

  • Power sequencing
  • Rail requirements and sequencing challenges
  • Handling high-current transient loads
  • Separate analog/digital power considerations

DDR Design

  • DDR4/LPDDR4 layout guidelines
  • Length matching and impedance requirements
  • Signal integrity concerns
  • Recommendations for stack-up and routing

Boot and Storage

  • eMMC boot flashing
  • QSPI NOR usage
  • Boot mode configuration
  • Reliable field update strategy

Clocking

  • Oscillator requirements
  • Jitter-sensitive interfaces
  • Clock tree recommendations

Thermal Design

  • Expected thermal challenges with Linux + RTOS workloads
  • Need for heatsink/fan or passive cooling
  • PCB thermal considerations

2. Linux + RTOS Coexistence Architecture

I need guidance on the recommended software architecture for heterogeneous processing on TDA4VM.

Questions:

  • Best practice for partitioning tasks between Linux and RTOS?
  • Recommended IPC mechanism:
    • RPMsg?
    • Shared memory?
  • Synchronization methods between A72 and R5F cores
  • Latency expectations for Linux ↔ RTOS communication
  • Recommended approach for deterministic motor control

3. Sensor Integration

Planned sensors include:

  • IMU
  • Magnetometer/Compass
  • Altimeter/Barometer

Questions:

  • Should sensor fusion run entirely on R5F?
  • Best interfaces:
    • SPI vs I2C for IMU
  • Recommendations for timestamp synchronization
  • Handling high-frequency sensor acquisition under RTOS

4. Motor Control Architecture

The RTOS side will drive motors in real time.

Guidance needed on:

  • Using PWM modules on TDA4VM
  • Encoder interfacing options
  • Real-time latency expectations
  • Isolation/protection recommendations
  • Whether external motor-control MCU is recommended or TDA4VM RTOS cores are sufficient

5. Software Development Flow

I would appreciate recommendations regarding:

SDK / Tools

  • Preferred Processor SDK version
  • Build environment recommendations
  • Yocto vs Buildroot
  • CCS usage for debugging RTOS cores

Boot Flow

  • SPL/U-Boot considerations
  • Multi-core boot process
  • Remoteproc usage
  • Flashing of OS through USB on eMMC.

Debugging

  • JTAG recommendations
  • Early boot debugging methods
  • Trace/logging best practices

6. Functional Safety / Reliability

Since this is intended for a mission-critical embedded application, I would also like suggestions on:

  • Watchdog implementation strategy
  • Brownout handling
  • Safe recovery mechanisms
  • Logging and crash diagnostics
  • Power-fail handling

7. Bring-Up Recommendations

Would like advice on:

  • Minimum hardware required for first bring-up
  • Common mistakes during custom board development
  • Signal integrity validation steps
  • Recommended bring-up checklist

8. Reference Designs and Documentation

Please share any:

  • Reference schematics
  • Design guide
  • Proven PCB stack-up examples
  • DDR routing examples
  • Linux + RTOS examples
  • IPC demos
  • Motor-control reference implementations

Current Understanding / Planned Setup

Tentative interfaces planned:

  • eMMC + NoR flash x 1
  • MIPI CSI2 x 1
  • Ethernet x 2
  • SPI x 1
  • I2C x 1
  • UARTs ( LINUX x 2 , RTOS x 2)
  • USB x 1
  • PWM x 4
  • Possibly PCIe in future revisions

OS plan:

  • Linux on A72
  • FreeRTOS or TI-RTOS on R5F

If anyone has experience building a custom board with TDA4VM and deploying Linux + RTOS heterogeneous systems for robotics/autonomous applications, I would greatly appreciate architecture suggestions, lessons learned and pitfalls to avoid.

Thank you.

  • I think you will have difficulty getting answers with a single post requesting information covering wide range of topics.  Understand these questions are routed to specific domain owners - please try to organize your questions with that understanding.  Below is some info to get you started on hardware/PCB design topics.

    Have you researched the information available on TI.com?  Much of the introductory information should be available there.

    Power Architecture:

    - recommend reviewing TI's EVMs available (J721EXSOMXEVM, Design files) and power supply application notes (PDN-1A, PDN-0B)

    - Power sequencing documented in data manual

    - Load transients, there are impedance targets documented for critical power domains

    - handling of analog power, see TI's EVM and power supply application notes (recommend follow example designs)

    DDR Design

    - Review existing application note (LPDDR4 PCB Guidelines ) and follow TI's EVM as close as possible (as it has been validated)

    High Speed Signal

    - Review existing application note (High Speed PCB Guidelines)

    Schematic Design Review Checklist (Link)