This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: AM62L: Testing Codesys

Other Parts Discussed in Thread: AM62L, AM62P

This thread is a followup to thread
AM62L: AM62L Real-time Performance Issue 

Hi Nick,

Thank you very much for your support.

I have applied the above DDR QoS configuration in the actual operating scenario, where Codesys runs with a 1ms cycle and controls four motors. After a 6-hour test, the jitter value displayed on the Codesys host ranged from -132 to 139. Unfortunately, I did not observe any performance improvement. Our project will halt motor control and stop data collection once the jitter exceeds the threshold of [-100, 100].

Based on the cyclictest data you provided, the configuration with  -i 1000  shows significant optimization. The jitter has dropped from over 200 microseconds to above 100 microseconds.

Regards,

Xi

  • Hi Xi,

    Our internal Ethercat expert has the following 3 points may need align with you, thanks.

    • For the A53 core Codesys is running, are there any other peripheral interrupts (apart from ethernet IRQ) on this core also?
    • Are Ethernet IRQ and Codesys running on the same A53 core?
    • Are Ethernet IRQ threads priority the same as Codesys EtherCAT_Task?

    Thanks,

    Kevin

  • Hi Kevin,

    There are eight Ethernet TX interrupts in the CODESYS application scenario. Four of them are assigned to CPU0, which shares the same core as CODESYS, while the other four are on CPU1, running alongside the EtherCAT task.

    All interrupt threads have a priority of -51, and the EtherCAT task thread runs at priority -57. Apart from these, only the arch_timer interrupt is observed, with no other peripheral interrupts present.

    We also tried pinning all Ethernet interrupts to CPU0, but tests showed this brought no improvement to real-time performance.

  • Hi Xi,

    1. How did youverify the 4 TX interrupts are truly mapped to port connected to EtherCAT network and other 4 TX interrupts mapped to the other port?
    2. Can you try setting all RX and TX interrupts to same priority as EtherCAT_Task 
    3. How are you mapping the RX interrupt(s)?

    -Daolin

  • Hi Daolin, 

    The previous description regarding interrupt relationships was incorrect. I have reorganized my interrupt mapping situation. Currently, under my CPU, there are 8 ethernet-tx interrupts and 1 ethernet-rx interrupt (corresponding to two hardware network ports: ethernet & ethercat). I confirmed this by connecting only ethercat or only ethernet. Under ethercat business functions, only the tx6 interrupt is frequently generated, so I bound it to cpu1 together with the ethercat task and adjusted it to the same priority of -57.

    As for the ethernet-rx interrupt, it is generated when either the ethernet port or the ethercat port is plugged in, so I have bound it to cpu0 with a priority of -51.

    I bound the other ethernet interrupts to cpu0 with unadjusted priority, all remaining at -51. I will continue running until tomorrow to see the results of this modification.

    By the way, regarding the reason for changing my CODESYS application from 1ms 4-axis to 8-axis: our product's ultimate goal is 1ms 8-axis control. Previously, when verifying jitter performance with 4-axis, the results were not satisfactory, so we didn't increase the load to the final target. Now, after configuring core-level DDR QoS and the kernel configuration CONFIG_VIRT_CPU_ACCOUNTING_GEN, the CODESYS jitter has improved to [-89, 90] (tested over 24 hours), so I switched to the final target of 8-axis. However, the above configuration doesn't show significant optimization for 8-axis; the jitter situation is similar to that under cyclictest simulated load.

    Regards,

    Xi

  • Hello Xi, 

    By the way, regarding the reason for changing my CODESYS application from 1ms 4-axis to 8-axis: our product's ultimate goal is 1ms 8-axis control. Previously, when verifying jitter performance with 4-axis, the results were not satisfactory, so we didn't increase the load to the final target. Now, after configuring core-level DDR QoS and the kernel configuration CONFIG_VIRT_CPU_ACCOUNTING_GEN, the CODESYS jitter has improved to [-89, 90] (tested over 24 hours), so I switched to the final target of 8-axis.

    Thanks for this clarification. Let's see the results of your IRQ mapping to see if that helps improve jitter.

    I confirmed this by connecting only ethercat or only ethernet. Under ethercat business functions, only the tx6 interrupt is frequently generated, so I bound it to cpu1 together with the ethercat task and adjusted it to the same priority of -57.

    Please ensure that you have disabled irqbalance so that the irq mapping doesn't get changed by the OS during runtime. If irqbalance is still enabled, even if you mapped irqs to a specific cpu, the OS could still change the core the irq is run on.

    As for the ethernet-rx interrupt, it is generated when either the ethernet port or the ethercat port is plugged in, so I have bound it to cpu0 with a priority of -51.

    One note about your IRQ mapping, since ethercat port is also using the same ethernet-rx interrupt, mapping to non-ethercat cpu core (cpu1) might not help with jitter. There is a way to create two separate RX flows/queues to introduce two separate ethernet-rx interrupts (see below). Once you enable two ethernet-rx interrupts, you can then bound the rx interrupt for ethercat port to cpu1 (with same priority as EtherCAT_Task -57) and give it a test.

    ethtool -l eth0
    ethtool -l eth1
    ifconfig eth0 down
    ifconfig eth1 down
    sleep 2
    ethtool -L eth1 rx 2
    ifconfig eth0 up
    ifconfig eth1 up
    ethtool -l eth0
    ethtool -l eth1
    sleep 2
    cat /proc/interrupts | grep rx

    -Daolin

  • Hi Daolin,

    Yesterday's test results: 1ms 8-axis, test duration 16h, jitter range [-136, 136].

    I have confirmed that irqbalance is not configured;

    Regarding the creation of ethernet-rx queues, I encountered a problem. When attempting to generate two rx queues, the kernel reports an error, and the log situation is as follows:

    root@am62xx-evm:/# ethtool -l eth1
    Channel parameters for eth1:
    Pre-set maximums:
    RX: 8
    TX: 8
    Other: n/a
    Combined: n/a
    Current hardware settings:
    RX: 1
    TX: 8
    Other: n/a
    Combined: n/a
    root@am62xx-evm:/# ethtool -l eth0
    Channel parameters for eth0:
    Pre-set maximums:
    RX: 8
    TX: 8
    Other: n/a
    Combined: n/a
    Current hardware settings:
    RX: 1
    TX: 8
    Other: n/a
    Combined: n/a

    root@am62xx-evm:/# ifconfig eth0 down
    [63581.120218] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
    root@am62xx-evm:/# ifconfig eth1 down
    [63584.617452] am65-cpsw-nuss 8000000.ethernet eth1: Link is Down
    root@am62xx-evm:/# 2026-01-13T20:10:25.990Z: Cmp=CmpRouter, Class=1, Error=0, Info=5, pszInfo= Network interface <interface>ether 2</interface> unregistered
    root@am62xx-evm:/# ethtool -L eth1 rx 2
    [63604.110907] __cma_alloc: 11 callbacks suppressed
    [63604.110925] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38
    [63604.110931] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.137523] cma: __cma_alloc: reserved: alloc failed, req-size: 17 pages, ret: -38
    [63604.137547] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.157844] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38
    [63604.157867] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.173800] cma: __cma_alloc: reserved: alloc failed, req-size: 17 pages, ret: -38
    [63604.173818] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.195817] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38
    [63604.195837] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.212817] cma: __cma_alloc: reserved: alloc failed, req-size: 17 pages, ret: -38
    [63604.212836] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.232819] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38
    [63604.232843] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.252837] cma: __cma_alloc: reserved: alloc failed, req-size: 17 pages, ret: -38
    [63604.252856] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.274813] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38
    [63604.274832] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.293814] cma: __cma_alloc: reserved: alloc failed, req-size: 17 pages, ret: -38
    [63604.293834] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.315821] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.326816] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.341814] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.353867] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.366822] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.377814] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.393820] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.394190] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 96
    [63604.412087] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.424816] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages
    [63604.424916] am65-cpsw-nuss 8000000.ethernet: Failed to get rx dma irq -22
    netlink error: Invalid argument

  • Hello Xi, 

    Apologies for the delay in response.

    Just to confirm, SDK version in use is ti-processor-sdk-linux-rt-am62lxx-evm-11.02.08.02-Linux-x86-Install.bin, with a kernel version of 6.12.57 on your setup? What is the result of your "uname -a"? My understanding is that enabling multiple RX flows should be possible on this version of the SDK 

    [63604.110925] cma: __cma_alloc: reserved: alloc failed, req-size: 2 pages, ret: -38

    From my understanding, -38 (-ENOSYS) indicates the operation is not available for the CMA (contiguous memory allocator) region. Indicates the driver is attempting per-channel DMA allocations from the CMA region named "reserved", which rejects then with ENOSYS - the region is inaccessible to this driver (likely reserved for another device in the DTS). What is your DTS? Does it differ from the TI default DTS for AM62L EVM?

    [63604.293834] cma: number of available pages: 8192@0=> 8192 free of 8192 total pages

    Indicates memory is still 100% free, indicating the -38 issue is likely a permission/configuration problem, not because there is no memory.

    [63604.394190] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 96

    Indicates that the CPSW driver was able to move past DMA buffer allocation and configured a UDMA flow ID base of 96 (TI-specific DMA routing identifier)

    [63604.424916] am65-cpsw-nuss 8000000.ethernet: Failed to get rx dma irq -22

    However, this log then indicates no IRQ was obtained for the 2nd RX DMA channel which is necessary for being able to separate out the RX flows for each port to separate cores. 

    I'm also trying to get a colleague to verify these commands on AM62L SDK 11.2 to see if this issue might be unique to AM62L or not.

    -Daolin

  • Hello Xi,

    Apologies for the delay in response.

    Please use the below patch to enable multiple RX flows using the script I previously provided. I've tested this on SDK 11.2 RT-Linux on an AM62L EVM and this patch appears to work.

     

    diff --git a/arch/arm64/boot/dts/ti/k3-am62l-main.dtsi b/arch/arm64/boot/dts/ti/k3-am62l-main.dtsi
    index 60f394b4eb983..9a480b39da3c0 100644
    --- a/arch/arm64/boot/dts/ti/k3-am62l-main.dtsi
    +++ b/arch/arm64/boot/dts/ti/k3-am62l-main.dtsi
    @@ -803,7 +803,22 @@ main_pktdma: dma-controller@485c0000 {
                            <0 0 77 &gic500 0 0 GIC_SPI 513 IRQ_TYPE_LEVEL_HIGH>,
                            <0 0 78 &gic500 0 0 GIC_SPI 514 IRQ_TYPE_LEVEL_HIGH>,
                            <0 0 79 &gic500 0 0 GIC_SPI 515 IRQ_TYPE_LEVEL_HIGH>,
    -                       <0 0 96 &gic500 0 0 GIC_SPI 484 IRQ_TYPE_LEVEL_HIGH>;
    +                       <0 0 96 &gic500 0 0 GIC_SPI 484 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 97 &gic500 0 0 GIC_SPI 485 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 98 &gic500 0 0 GIC_SPI 486 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 99 &gic500 0 0 GIC_SPI 487 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 100 &gic500 0 0 GIC_SPI 488 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 101 &gic500 0 0 GIC_SPI 489 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 102 &gic500 0 0 GIC_SPI 490 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 103 &gic500 0 0 GIC_SPI 491 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 104 &gic500 0 0 GIC_SPI 492 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 105 &gic500 0 0 GIC_SPI 493 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 106 &gic500 0 0 GIC_SPI 494 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 107 &gic500 0 0 GIC_SPI 495 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 108 &gic500 0 0 GIC_SPI 496 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 109 &gic500 0 0 GIC_SPI 497 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 110 &gic500 0 0 GIC_SPI 498 IRQ_TYPE_LEVEL_HIGH>,
    +                       <0 0 111 &gic500 0 0 GIC_SPI 499 IRQ_TYPE_LEVEL_HIGH>;
            };
     
            cpsw3g: ethernet@8000000 {

    Once verified that this patch enables multiple RX flows you can try the below two tests to see if it will also improve jitter on your system:

    1. (Previously described test) Enable two ethernet-rx interrupts, you can then bound the rx interrupt for ethercat port to cpu1 (with same priority as EtherCAT_Task -57) and give it a test (I saw reduction to ~80us jitter on AM62P with 6 axes)

    2. Completely isolate the CODESYS IDE tasks and IDE port RX/TX interrupts from CODESYS EtherCAT task and ECAT port RX/TX interrupts, below is a starting point to do this (what I had used) (I saw reduction to ~76us jitter on AM62P with 6 axes)

    1. Isolate CPU 1,2,3 with the following
    OLD: optargs=vt.global_cursor_default=0 isolcpus=3 rcu_nocbs=3 nohz_full=3 irqaffinity=0
    NEW: optargs=vt.global_cursor_default=0 isolcpus=1,2,3 rcu_nocbs=1,2,3 nohz_full=1,2,3 irqaffinity=0
    2. Add the contents below "[SysCpuMultiCore]" in CODESYSControl.cfg (to move as many codesys non-EtherCAT child tasks to core 1)
    3. Run v3-add-rt-tunings.sh to move IDE Rx/Tx to CPU1 and ECAT Rx/Tx to CPU2
    4. Ensure CODESYS IDE had pinned EtherCAT_Task to CPU3
    Recap of separation:
    1. CPU0- housekeeping
    2. CPU1- IDE Rx/Tx + IDE application
    3. CPU2- ECAT Rx/Tx
    4. CPU3- Codesys ECAT task

    CODESYSControl.cfg

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/v3_2D00_add_2D00_rt_2D00_tunings.sh

    -Daolin

  • Hi Daolin,

    Thanks for the support and the patch (customer has modified the rx position as you suggested above) here, please see below updates:

    For 1ms cycle time, 4 axis, 24 hour test: the jitter improves from 86us to 73us

    However, for 1ms cycle time, 8 axis, still having the problem exceeding the 1ms cycle time, after running about 30 minutes, the cycle time will increase to about 1200us exceeding the 1ms cycle time, and the customer's application will stop immediately if cycle time exceed 1ms, so there is also no way to verify if there is jitter improvement in 8 axis scenario.

    Customer has management level discussion, due to the huge additional cost, they refuse to consider XDP options.

    So currently we need find a way helping customer solve the cycle time issue in 8 axis.

    Thanks,

    Kevin

  • Hi Kevin,

    However, for 1ms cycle time, 8 axis, still having the problem exceeding the 1ms cycle time, after running about 30 minutes, the cycle time will increase to about 1200us exceeding the 1ms cycle time, and the customer's application will stop immediately if cycle time exceed 1ms, so there is also no way to verify if there is jitter improvement in 8 axis scenario.

    Since the current blockage to testing jitter improvement on 8-axes case is cycle time, as a temporary test, can customer increase configured cycle time to 2ms and check jitter with the rx flow configuration?

    -Daolin

  • Hi Daolin,

    Customer feedback that after increasing configured cycle time to 2ms for 8 axis, the result is below under 24 hours testing:

    Max Cycle Time: 1300us ~ 1400us

    Max Jitter: 80 ~ 90us

    Please let us know if there is anything else could further improve cycle time, thanks.

    Kevin

  • Hi Kevin, 

    1. Did the suggested changes (DDS QoS and RX flow separation) prove helpful for 8-axis jitter case?

    2. We are working to profile what is contributing to cycle time to give some answers to whether there is something further to improve on from cycle time perspective beyond XDP zero copy. As discussed in our meeting, before profiling I will try to prioritize benchmarking further with XDP zero copy to provide more datapoint on benefits of XDP zero copy on cycle time. 

    Please be aware my responses will be delayed until August 24th since I will be out of office until then.

    -Daolin

  • Hi Daolin

    Yes, both DDR QoS & RX Flow Separation are helpful for 4-axis & 8-axis jitter.

    Let's focus on cycle time reduction after your return.

    Thanks,

    Kevin

  • Hi Kevin, 

    As Daolin mentioned, they'll return to office on August 25th. Please expect a delayed response.