This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6411: Down Clocking Min Value

Part Number: AM6411

As seen from the datasheet below, only a typical number is given for the device input clock.

What is minimum value the device can be clocked?

In the past, some Sitara and DSP devices could go all the way down to 0 Hz.

image.png

  • Hello Joe,

    The AM6411 requires a 25 MHz reference clock on its MCU_OSC0 input. This clock is mandatory and is the only crystal frequency that the device supports – there is no lower‑frequency option. In other words, the minimum (and typical) input‑clock frequency is 25 MHz. 

    Best Regards,

    Borislav Lazarkov