The DM814x Wiki doesn't appear to have Codec availability listed:
http://processors.wiki.ti.com/index.php/Category:DM814x
I'd like to know if 1080p at 60fps is currently supported in the DM814x devices.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The DM814x Wiki doesn't appear to have Codec availability listed:
http://processors.wiki.ti.com/index.php/Category:DM814x
I'd like to know if 1080p at 60fps is currently supported in the DM814x devices.
Yes, 1080p @ 60 fps is supported on DM814x devices.
It would need HDVICP2 to be clocked at around 450 - 500 Mhz depending on the use case.
For ex: Consumer class applications would need HDVICP at 450 Mhz, while Broadcast applications would need HDVICP at 500+ Mhz.
Regards,
Pavan
Hi,
Currently with 450Mhz of IVA-HD, we can run 1080p60+D130 and MJPEG 1080p5 .
TO run only single channel of 1080p60, 400Mhz of IVA-HD is good enough.
What is the usecase you are planning?
Regards,
Raghu
Thanks for the responses. Is there any documentation available that shows OS support for the HDVICP2 hardware?
Raghu, if you'd like you can email me regarding the application. I'd rather not disclose on the forums.