This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: Error code in XDS110

Part Number: TMDSEMU110-U

Dear everyone,

 

I have issue with TMDSEMU110-U programming on TMS320F280048 and  TMS320F280040 failed code as below. Do you know root cause refer error code?

 

Waiting for 0 seconds, press a key to continue ...
DSLite version 10.0.0.1942
Configuring Debugger (may take a few minutes on first launch)...
        Initializing Register Database...
        Initializing: IcePick_C_0
        Executing Startup Scripts: IcePick_C_0
        Initializing: C28xx_CPU1
        Executing Startup Scripts: C28xx_CPU1
Connecting...
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
error: C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
Loading Program: D:\BMW_BTLD_STANDARD\BMW_PHEV_11KW\EAP00500801D1\FBL_D1R0P0T0\LV DCDC CTRL\DCDCLlcx40\user_files\images\Bmw_DcDcLlcx40_FBL.hex
        Preparing ...
        0 of 7548 at 0x80000
warning: C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable.  These regions will not actually be written to the target.  Check your linker configuration and/or memory map.
error: C28xx_CPU1: File Loader: Verification failed: Values at address 0x80000@Program do not match Please verify target memory and memory map.
        Finished
Failed: File: D:\BMW_BTLD_STANDARD\BMW_PHEV_11KW\EAP00500801D1\FBL_D1R0P0T0\LV DCDC CTRL\DCDCLlcx40\user_files\images\Bmw_DcDcLlcx40_FBL.hex: a data verificati

 

Thank you in advance.

Thanapol S.