Part Number: SK-AM62A-LP
Hello Engineer,
I am working in OD application.
input0:
source: /opt/video/sample.mp4
format: h264
width: 1280
height: 720
framerate: 20
loop: True
loop is true still after the video end it will stuck. Below is the GST_DEBUG level 3 log when after EOS.
0:03:07.665746600 2387 0xffff54136c60 WARN bufferpool gstbufferpool.c:1246:default_reset_buffer:<v4l2h264dec0:pool0:src> Buffer 0xffff54350dd0 without the memory tag has maxsize (0) that is smaller than the configured buffer pool size (1382400). The buffer will be not be reused. This is most likely a bug in this GstBufferPool subclass
0:03:07.665859455 2387 0xffff54136c60 WARN bufferpool gstbufferpool.c:1246:default_reset_buffer:<v4l2h264dec0:pool0:src> Buffer 0xffff5800e020 without the memory tag has maxsize (0) that is smaller than the configured buffer pool size (1382400). The buffer will be not be reused. This is most likely a bug in this GstBufferPool subclass
0:03:07.665927894 2387 0xffff54136c60 WARN bufferpool gstbufferpool.c:1246:default_reset_buffer:<v4l2h264dec0:pool0:src> Buffer 0xffff5800e3f0 without the memory tag has maxsize (0) that is smaller than the configured buffer pool size (1382400). The buffer will be not be reused. This is most likely a bug in this GstBufferPool subclass
0:03:07.665984936 2387 0xffff54136c60 WARN bufferpool gstbufferpool.c:1246:default_reset_buffer:<v4l2h264dec0:pool0:src> Buffer 0xffff5800e7c0 without the memory tag has maxsize (0) that is smaller than the configured buffer pool size (1382400). The buffer will be not be reused. This is most likely a bug in this GstBufferPool subclass
Also app crashes sometimes, I got an understanding that cma memory becomes starved but the whole system uses about 600MB of memory at that time. Terminal log is [ERROR] Error pulling frame from GST Pipeline.
Best Regards,
Sajan