7853.720x576_vlc.txt1780.720x576_vlc.txt
Hi,
I have ran the mpeg2 dec for ezk_5_03_01_15 .
I observe there is a frame skip and also in between of decoding some of the frames prints "OMX error ID = 0x8000100b" , corrupted bitstream.
The input bitstream is attached as .txt file.
Please find the teraterm log below, the original bitstream contains 18 frames :
root@dm816x-evm:~# ./decode_a8host_debug.xv5T -i 720x576_vlc.m2v -w 720 -h 576
-o out.yuv -c mpeg2
input file: 720x576_vlc.m2v
width: 720
height: 576
output_file: out.yuv
codec: mpeg2
Decoder example
===============================
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
Iteration 0 - Start
allocating field buffer
calling getHandle
Output port buffer size: 663552
state IDLE
state execute
etb / ftb done
Component generated error; OMX error ID = 0x8000100b
frame 1 decoded
frame 1 displayed
frame 2 displayed
frame 3 displayed
frame 4 displayed
frame 2 decoded
frame 3 decoded
frame 4 decoded
frame 5 decoded
frame 5 displayed
frame 6 displayed
frame 7 displayed
frame 8 displayed
frame 6 decoded
frame 7 decoded
frame 8 decoded
frame 9 decoded
frame 9 displayed
Component generated error; OMX error ID = 0x8000100b
Component generated error; OMX error ID = 0x8000100b
frame 10 displayed
frame 11 displayed
frame 12 displayed
frame 10 decoded
frame 11 decoded
frame 12 decoded
frame 13 decoded
frame 13 displayed
frame 14 displayed
frame 15 displayed
frame 16 displayed
No more to read
frame 14 decoded
Tearing down the decode example
Error OMX_ErrorUndefined: WaitForState has timed out
Decoder Test End
Regards
Pujari