This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: systemd-shutdown: Failed to disable hardware watchdog

Part Number: DRA821U
Other Parts Discussed in Thread: DRA821

Hi Team,

I am working on a DRA821 processor-based custom board running Linux. During a normal reboot ('reboot' command from Linux userspace), the system shuts down successfully and eventually restarts. However, the following messages are consistently observed during the shutdown sequence:


[   31.577965] watchdog: watchdog0: nowayout prevents watchdog being stopped!
[   31.584860] watchdog: watchdog0: watchdog did not stop!
[   31.600296] systemd-shutdown[1]: Using hardware watchdog 'K3 RTI Watchdog', version 0, device /dev/watchdog0
[   31.610151] systemd-shutdown[1]: Modifying watchdog hardware timeout is not supported, reusing the programmed timeout.
[   31.620847] systemd-shutdown[1]: Watchdog running with a hardware timeout of 1min.
...
[   31.801415] watchdog: watchdog0: nowayout prevents watchdog being stopped!
[   31.808288] systemd-shutdown[1]: Failed to disable hardware watchdog, ignoring: Device or resource busy
[   31.817670] watchdog: watchdog0: nowayout prevents watchdog being stopped!
[   31.824531] watchdog: watchdog0: watchdog did not stop!
...
[   31.839399] systemd-shutdown[1]: Rebooting.
[   31.862137] reboot: Restarting system


The system reboots successfully after these messages.

Why does the following message appear during reboot?

   systemd-shutdown[1]: Failed to disable hardware watchdog, ignoring: Device or resource busy

Please let us know whether this behavior is expected and if any additional configuration changes are required.

Regards,
Ashwini A