Part Number: DRA821U
Other Parts Discussed in Thread: DRA821
Hi I have a question regarding DRA821U4's supported MAC interfaces on Ethernet Switch.
Does this switch support 10G QXGMII on this switch? I know that this mode sometimes has different names depending on the vendor (like USXGMII) and so on, but I'm in particular interested in 10Gb with 4 aggregated ports over single serdes
By comparsion:
This is e.g. information from LS1028A
"10G-QXGMII allows 4 TSN Switch MACs to share a single SerDes lane and negotiate speeds up to 2.5 Gbps per
link. It is connected to the 4 switch ports and supports each port negotiating rates of 10M, 100M, 1G, or 2.5G."
I of course checked the datasheet and saw this:
DRA821U4 CPSW5G supports the following instances, signals, and modes of operation:
• PORT1 Signals: RMII1/RGMII1/SGMII1, Modes: One of 5Gb, 10Gb USXGMII/XFI, 2.5 Gb SGMII/XAUI, 1Gb SGMII, 1Gb RGMII,
100Mb RMII, 5Gb QSGMII
• PORT2 Signals: RMII2/RGMII2/SGMII2, Modes: One of 2.5 Gb SGMII/XAUI, 1Gb SGMII, 1Gb RGMII, 100Mb RMII, 5Gb QSGMII
• PORT3 Signals: RMII3/RGMII3/SGMII3, Modes: One of 2.5 Gb SGMII/XAUI, 1Gb SGMII, 1Gb RGMII, 100Mb RMII, 5Gb QSGMII
• PORT4 Signals: RMII4/RGMII4/SGMII4, Modes: One of 2.5 Gb SGMII/XAUI, 1Gb SGMII, 1Gb RGMII, 100Mb RMII, 5Gb QSGMII
• QSGMII mode combines all four internal ports of the CPSW onto a single SERDES lane. Each port in this mode operates at 1-Gb
full duplex
– Any one of the port signals SGMII1:4 can be selected for this SERDES connectivity where upon the non-selected signals are
unused by the CPSW
but just want to confirm as there is USXGMII mentioned abve but not sure if capable of aggregating 4 ports over single serdes as described in my question.
Does DRA821 support something like this? Is there ANY DRA821 variant that would support this mode?