Other Parts Discussed in Thread: AM1808
I am working with an AM1808 on a custom board that seems to be in a funny state that won't fully boot. I am building my application with gcc. When I try to Run->Load->Load Program... it copies my application about 75% of the way and then there is an error stating it can't copy to some DDR address. I tried running the gel script Core_100MHz_mDDR_102MHz. Then I am able to fully copy the application, but it gets stuck in a loop in ROM. See the green lines in the disassembly.

I also tried reducing the size of my application to almost nothing. In that case I can actually step into main, but I can only run about 2 lines of code before it hangs.
Any ideas on what I can look for? Registery settings?
Sam