Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: J784S4XEVM, AM69A, AM68A
Hello TI Experts,
I have both the J784S4XEVM and SK-AM69A boards on which I want to evaluate SW performance. Can both platforms be supported with a single Processor SDK Linux installation? I lack the disk space to support full Yocto builds on both SDKs individually, and I was wondering whether a single installation can handle both boards. The SDK documentation seems to hint at that by setting the MACHINE variable, e.g.,
MACHINE=<machine> bitbake <target>
Then again, the J784S4 SDK has 11.02.00.04 as latest release, while the AM69A SDK only goes up to 11.00.00.08. So, before I would start the exercise with a single SDK installation, I would like confirmation whether or not a single installation is sufficient. And if so, which SDK version would be most suitable for that?
Kind regards,
Christophe