Hi all,
I try to create a USB communication (Bulk), i use ccs 5.1, Starterware 1.10.02.02 and SYSBIOS 6.
I joint my USB.c file, its mostly the same as the usb_dev_bulk.c but without the LCD code.
I want to create a task with SYSBIOS that will be run my function : void USB(void) (see in my USB.c) This task will manage all the traffic on the USB. The problem is when i create my task and associate the function void USB(void) to the task, i got this error:
undefined first referenced
symbol in file
--------- ----------------
USBBufferDataWritten ./USB.obj
USBBufferFlush ./USB.obj
USBBufferInfoGet ./USB.obj
USBBufferInit ./USB.obj
USBBufferSpaceAvailable ./USB.obj
USBDBulkInit ./USB.obj
g_pucUSBRxBuffer ./USB.obj
g_pucUSBTxBuffer ./USB.obj
g_sBulkDevice ./USB.obj
g_sRxBuffer ./USB.obj
g_sTxBuffer ./USB.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "Plasma_Detek_DSP.out" not
built
Does SYSBIOS support the Starterware function?