Part Number: 66AK2H06
Hello experts,
We are having issues with rx align errors in 1Gb ethernet and using 66AK2H06 SOC.
My question concerns the initial calibration of serdes during powerup. The silicon errdata SPRZ402F has on pages 84 & 85 a section 'SerDes Fails to Adapt RX BOOST Equalization'. There it explains that the calibration is not done if 8/10b decoding is used. The peripherals listed does not show the 1.25GHz SGMII but the decoding is exactly same 8/10b in 1Gb Ethernet.
According to SPRUHO3A, section 15.3 describes the initial calibration and after PHY startup sequence is complete and it will be done only once. But, taking the silicon errdata into account, is the SOC RX calibrated at all since the 8/10b decoding is being used?